Tape rotation for LTV-352T

------Question for LTV-352T Please Put your question below------
What is the rotation in tape for LTV-352T? In DS I found LTV-352T-TP and LTV-352T-TP1
Which of the above is for LTV-352T?

Welcome to our community!

please see the screenshot of LTV-352T series 201610 datasheet from Lite-ON Inc. with Pin 1 indicated in GREEN

and the screenshot of LTV-352T series 201610 datasheet from Lite-ON Inc. with Pin 1 indicated in GREEN as orientation in the tape for the Pb-free or lead free option as well on the opposite site of the holes [only the 1 indicates that the parts are turned]: LTV-352T-TP & LTV-352TP

1 Like