------Question for RUTX50000200 Please Put your question below------
Before placing an order, please confirm the following:
-
Exact manufacturer part number:
→ RUTX50000200 (North America version)
-
Region compatibility:
→ Supports Canada/USA 5G and LTE bands (not EU version)
-
Modem specification:
→ 5G with LTE Cat20 fallback
-
WiFi:
→ WiFi 6 (802.11ax)
-
Power input:
→ Compatible with direct 24V DC (approx. 9–50V range)
-
Failover capability:
→ Dual SIM + WAN failover (Ethernet ↔ cellular)
-
Firmware:
→ Standard Teltonika RutOS (not carrier-locked)
-
Availability:
→ In stock or confirmed lead time
-
Verification:
→ Can you confirm this is NOT SKU 00000 / 00100 / 00300?
Thank you,
Louis
------Question for RUTX50000200 Please Put your question below------
Power cable (bare wire or adapter?)
Cellular antennas (how many?)
WiFi antennas (how many?)
Mounting hardware?
I combined your two posts, since they’re on the same part number there is no need to create a separate thread.
The manufacturer does not list these are for the US or Canada and I don’t see that they have an FCC license available for any of these parts.
The regions they specify are as follows:
Thank you for the answer.
I understand that the listed SKUs (RUTX50000000 / 00100 / 00200 / 00300) mainly refer to power supply variants and the modem configuration
However, my requirement is very specific: I need confirmation whether any RUTX50 variant is officially supported or certified for use in Canada or the United States (FCC / ISED).
At this stage I am trying to determine if the RUTX5000200 is usable but not certified OR RUTX50*** should be avoided entirely for North America
There is not a RUTX50 variant that is officially supported or certified for use in Canada or the United States (FCC / ISED)
Their certifications can be found here: RUTX50 Industrial 5G Router
Thank you - It is now clear… will need something else in Canada