Transconductance

------Question for STF27N60M2-EP Please Put your question below------

gfs is not listed in this part’s datasheet.

Edit: Transconductance is answered HERE.

Hello stephen.franks,

I was unable to find the transconductance value on STMicroelectronics’s website, so I will be reaching out to them to see if they can advise. I will post here once I hear back.

Thank you,
Klint

Hi stephen.franks,

The forward transconductance is specified as the following:

image

It will vary depending on such things as temperature and applied VDS, and where along the ID/VGS curve one takes a measurement, but looking at the curve in Fig.5 on page 6 of the datasheet of the STF27N60M2-EP, it appears to be fairly linear between a VGS of about 4.6V and 5.4V.

So one can estimate transconductance as:

  • gfs = ΔID/ΔVGS ≈ (40A - 10A) / (5.4V - 4.6V) = 30A / 0.8V ≈ 37.5

This is of course a ball-park estimate based on looking at the graph, but I believe that estimate should be within 15% ~ 20% of the actual value.

1 Like

Greetings stephen.franks,

The response from the manufacturer supports what David_1528 posted earlier. Per the manufacturer:

A gfs value for this MOSFET can be obtained by taking the slope of the transfer characteristic, shown below in Fig. 5 (taken from the STF27N60M2-EP datasheet). In this case, VDS=20 V and the slope is taken at 1/2 the maximum ID value shown on the plot at ID=26A. When we find the slope at that point on the curve, gfs is obtained.

gfs = | dID / dVGS | at VDS=constant

At ID=26A, gfs is approximately 35.9 S for this transfer characteristic.

Regards,
Klint

1 Like