------Question for M12A12ML-12AFR-SBA05 Please Put your question below------
I need L-shaped M12 Male to Female connector for a line extension.
Can it be used for the Avia Rivox Lidar?
The plug of the Lidar is should be an M12 12PA-CODE fully shielded male connector that complies with the ICE61076-2-101 standard, model Finecables MA12MAHD12STXXXB14, All comply with IP67 protection requirements.
Hello hjkwon1 and welcome to the DigiKey TechForum.
From what I can see, it does not appear that M12A12ML-12AFR-SBA05 is shielded, and I see no mention of compliance with IEC61076-2-101 standards.
I did look through other A-Coded, 12 position, M12 cable assemblies we have and do not see that we have a shielded option, with an L-Shaped connector.
Hi hjkwon1,
The nearest product I could find to what you’re looking for would be this:
- 1404941 – M12 A-Coded Receptacle to Plug, Shielded, Straight, Length → 1.0m
- Meets IEC 61076-2-101 specifications
Hello,
Thank you for your response.
Actually, I need L-shaped tip similar to the product you suggest.
If you can find any suggestion, I would be happy to purchase it.
Best regards,
Hyungjin kwon
Unfortunately, I could not find any shielded options with the “L-shaped” tip.