Using the IL300 Linear Optocoupler for Isolated Voltage and Current Monitoring

The IL300 Linear Optocoupler is a linear optically isolated device designed for precision analog signal transfer. Its dual photodiode architecture allows implementation of closed-loop feedback circuits for improved gain stability and linearity.

This device is commonly used for isolated voltage monitoring and current sensing in industrial control systems. An automotive-qualified option is also available for high-reliability applications, it’s VOA300.

Figure 1: Typical closed-loop IL300 isolation amplifier configuration


Circuit Description

In this configuration, the IL300 is used as an isolation amplifier, where the gain can be individually adjusted:

  • U1 drives the LED input current (IF)
  • The primary feedback photodiode current (IP1) is monitored by U1, forming a servo loop that linearizes LED current
  • The secondary photodiode current (IP2) is optically coupled and proportional to IP1
  • U2 converts IP2 into an output voltage using R2

Due to matched photodiodes, transfer gain is set primarily by the external resistor ratio:

VOUT = (R2 / R1) * K3 * VIN

Where K3 is the photodiode transfer gain ratio specified in the datasheet, as:

K3 = K2 / K1 = (IP2 / IF) / (IP1 / IF) = IP2 / IP1


Input Signal Options (VIN)

The input node can be derived from several measurement sources:

  • Voltage drop across a current shunt resistor
  • Output of a high-voltage divider

This flexibility allows the same isolation topology to be used for both voltage and current
measurement.


Design Considerations

  • Select precision resistors to maintain gain accuracy
  • Account for K3 tolerance when calculating system error
  • Ensure op amp input bias current is low relative to photodiode current
  • Verify isolation voltage rating for the target application