Webinar: Siemens - SIRIUS Modular System goes digital with the NEW 3RC7

Siemens

Webinar Date: August 05, 2025

Key Takeaways

  • Understand the evolution of the SIRIUS Modular System with the new 3RC7 ILM
  • Learn how to integrate real-time load data directly into your automation systems
  • See a hands-on demo of 3RC7 hardware, wiring, and programming
  • Discover how to use collected data for predictive maintenance and performance analytics
  • Get expert insights on applying 3RC7 ILM in real-world manufacturing and control systems

Frequently Asked Questions

Do I need a specific module or can I put it directly on the network with a switch?

  • The Intelligent Link Module requires the ET 200SP. The gateway is needed in communication with the ILM.

Does it communicate with the remote via IO or network?

  • The Intelligent Link Module uses network for communication.

What makes the 3RC7 different from other digital load monitoring solutions?

  • The 3RC7 combines real-time current monitoring, predictive diagnostics, and multi-protocol communication in a compact, DIN-rail-mountable module. Unlike traditional and competitor solutions, it integrates seamlessly into the SIRIUS Modular System and supports PROFINET, EtherNet/IP, Modbus TCP, and OPC UA. Making it ideal for modern, connected control panels.

Can the 3RC7 be retrofitted into existing SIRIUS Modular System setups?

  • Yes! The 3RC7 is designed to be backward-compatible with existing SIRIUS Modular System components, making it easy to retrofit into existing panels. It enables digital monitoring and diagnostics without requiring a complete redesign.
  • Note: The 3RC7 is specifically designed for use with devices that feature spring-type connections, so compatibility should be verified based on the connection type of the existing setup.

Is special software or licensing required to configure the 3RC7?

  • No special license is required beyond the basic TIA Portal. The 3RC7 uses standard Siemens hardware and software blocks.

Can I use the MFCT tool to configure the 3RC7 when using protocols other than PROFINET (e.g., EtherNet/IP, Modbus TCP)?

  • The MFCT (Modular Function Configuration Tool) can be used for basic parameterization of the ET 200SP motor starters, including when using protocols like EtherNet/IP or Modbus TCP. However, when it comes to configuring the 3RC7 Intelligent Link Module, TIA Portal is required for full parameterization and integration.

Can the 3RC7 be used with any 3RV motor starter protector (MSP)?

  • The 3RC7 Intelligent Link Module is compatible with specific 3RV2 motor starter protectors particularly the 3RV23 series as they do not include overload protection.

  • The 3RC7 can also be used with 3RV21 MSPs, which do include overload protection. However, in this case, the overload setting on the 3RV21 must be set higher than the trip threshold configured in the 3RC7, to ensure proper coordination and avoid conflicts between the two protection mechanisms.

Referral Webinar Link

If you would like more information from this webinar, please review the details below.

DigiKey Webinar Center

DigiKey TechForum Webinar Posts

1 Like