------Question for NHD-C12832A1Z-FSW-FBW-3V3 Please Put your question below------
If I’m reading the data sheet:
correctly, the pin spacing is 1.5mm, and the pin width is 0.4mm by 0.3mm. For testing / debugging, I want to be able to connect without soldering these down, so I’m looking for a connector.
The only thing I can find that seems to have the same pin spacing and is a 1 by more than 16 is this:
https://www.molex.com/en-us/products/part-detail/2132273211?display=pdf
But I can’t even figure out what size pin that accepts.
Greetings,
I’d agree that the indicated pin cross section seems to be about 0.4x0.3mm; however they appear to be meant to facilitate through-hole mounting of the display only; a corresponding connector designed for purpose does not appear to be available.
It’s not clear to me that the molex part mentioned is even designed to accommodate a “pin” per-se; 1-353908-7 plus some of the associated contacts at the bottom of that product page might be a bit closer (corresponding pin contacts appear to be 0.5mm square) but it’s still a bodge and an inconvenient one at that.
Considering that the display in question is not that expensive, making oneself a permanent adapter to a standard 0.1" header seems the most reasonable way to go if one anticipates extended prototyping with the device.
1 Like
Also found that JST ZH connectors will fit the header. But they only come up to 10 pins and the 4 pin ones are common, so a set of 4 of those, trimmed and glued together are good enough for testing / debugging without having to make a PCB> I hope.