# What Is a Junction Field-Effect Transistor (JFET)?

**URL:** <https://forum.digikey.com/t/what-is-a-junction-field-effect-transistor-jfet/71931>\
**Category:** Discrete Semiconductor Products\
**Tags:** onsemi, terminology, transistors\
**Created:** [September 14, 2026, 9:16am UTC](https://forum.digikey.com/t/what-is-a-junction-field-effect-transistor-jfet/71931 "2026-09-14T09:16:01Z")\
**Posts on this page:** 1\
**Page:** 1

<div class="post-metadata">

**Author:** ![Angus\_Lai](https://sea2.discourse-cdn.com/digikey/user_avatar/forum.digikey.com/angus_lai/32/9895_2.png) [@Angus\_Lai](https://forum.digikey.com/u/Angus_Lai)\
**Post date:** [September 14, 2026, 9:16am UTC](https://forum.digikey.com/t/what-is-a-junction-field-effect-transistor-jfet/71931/1 "2026-09-14T09:16:01Z")

</div>

# What Is a Junction Field-Effect Transistor (JFET)?

A [**Junction Field-Effect Transistor (JFET)**](https://www.digikey.com/en/products/filter/transistors/jfets/288) is a **voltage-controlled semiconductor device** that operates using the **electric field effect**.

A JFET has three terminals:

- **Source (S)**
- **Drain (D)**
- **Gate (G)**

The structure of a JFET can be explained using an **N-channel JFET** as an example.

 ![image](https://global.discourse-cdn.com/digikey/original/3X/9/0/9080a987c613a84203da8d13998ee13ea9ef4b7c.png)

In an N-channel JFET, two electrodes are connected to the ends of an N-type semiconductor material, serving as the **Source** and **Drain**. Two heavily doped P-type regions are formed on opposite sides of the N-type material and connected together to form the **Gate**. This creates two back-to-back PN junctions.

The N-type region through which current flows is called the **channel** , forming an **N-channel JFET**.

A **P-channel JFET** , on the other hand, uses a P-type semiconductor as its channel region.

 ![image](https://global.discourse-cdn.com/digikey/original/3X/3/4/348ffb0cdf720ee6e4910d20776caa1e77bf5c75.png)

* * *

# Operating Principle of a JFET

A JFET controls current by varying the voltage between the **Gate** and **Source** (the reverse-bias voltage across the PN junction).

The depletion region of the PN junction expands into the more lightly doped semiconductor region, changing the effective cross-sectional area of the conductive channel and thereby controlling the current flow.

## 1. Zero Gate Bias: VGS = 0 V

There is no voltage difference between the gate and source, so the PN junction is at zero bias.

At this condition:

- The depletion region is at its narrowest.
- The N-type conductive channel is at its widest.
- The drain current ( **ID** ) reaches its maximum value ( **IDSS** , the saturation drain current).

 ![image](https://global.discourse-cdn.com/digikey/original/3X/1/9/195d7f650a08005989d834e9d6b5c9f2450c7aee.png)

* * *

## 2. Negative Bias: Vp \< VGS \< 0 V

The PN junction becomes reverse-biased.

As a result:

- The depletion region widens.
- The conductive channel narrows.
- The drain current ( **ID** ) decreases.

By adjusting **VGS** , the drain current can be precisely controlled.

 ![image](https://global.discourse-cdn.com/digikey/original/3X/e/6/e695fb0228e87cb72d12a251a8afa4b6e8549cdc.png)

* * *

## 3. Pinch-Off: VGS ≤ Vp

When the reverse-bias voltage reaches the pinch-off voltage ( **Vp** ):

- The depletion region expands further.
- The channel becomes completely pinched off.
- Current flow is nearly cut off.

 ![image](https://global.discourse-cdn.com/digikey/original/3X/9/3/937dc5feaf5b832bf2cbfc68b15a4d80c69c2cd4.png)

* * *

# Advantages of JFETs

Conventional JFETs (long-channel JFETs) are not primarily valued for high voltage or high current capability. Instead, they offer several unique advantages.

## 1. Extremely High Input Impedance

The gate-to-channel junction is a reverse-biased PN junction.

Under normal operation:

- Gate current is virtually zero.
- Loading on the preceding circuit stage is extremely small.

## 2. Excellent Low-Noise Performance

JFETs are **majority-carrier devices** (conduction by electrons or holes).

As a result:

- They do not exhibit the surface carrier scattering noise associated with MOSFET channels.
- They generate very little shot noise compared to BJTs (Bipolar Junction Transistors).

This makes them ideal for low-noise amplification applications.

## 3. Good Linearity

Within the saturation (constant-current) region:

- Drain current exhibits an approximately square-law relationship with **VGS**.
- The transconductance ( **gm** ) changes relatively smoothly.

This makes JFETs well suited for high-quality analog signal processing.

## 4. Unipolar Device With No Secondary Breakdown

JFETs do not suffer from the secondary breakdown phenomenon commonly associated with BJTs, providing greater stability and reliability.

## 5. Strong Resistance to Electrostatic Discharge (ESD)

Because the gate structure is a PN junction:

- The depletion region is located inside the semiconductor.
- The structure is generally more robust than the thin gate oxide used in MOSFETs.

As a result, JFETs typically offer better ESD tolerance.

* * *

# JFET Applications

## Typical Long-Channel JFET Applications

### 1. High-Impedance Sensor Interfaces

Examples include:

- Piezoelectric sensors
- Capacitive microphone preamplifiers

### 2. High-Fidelity Audio Equipment

Examples include:

- Phono preamplifiers
- Microphone preamplifiers
- Audio mixer input stages

These applications take advantage of the JFET’s low-noise and high-linearity characteristics.

### 3. Analog Switches and Sample-and-Hold Circuits

Because JFETs offer:

- Simple control characteristics
- Low on-resistance

They can also be used to create simple and stable constant-current sources.

### 4. RF Circuits

JFETs are still widely used in certain:

- VHF (Very High Frequency)
- UHF (Ultra High Frequency)

low-noise amplifier designs.

* * *

## Typical Short-Channel JFET Applications

### Static Induction Transistors (SITs)

Short-channel JFET structures are commonly used in **Static Induction Transistors (SITs)**.

* * *

# Example: onsemi MMBFJ201

The **[onsemi](https://www.digikey.com/en/supplier-centers/onsemi) [MMBFJ201](https://www.digikey.com/en/products/detail/onsemi/MMBFJ201/1049584)** can be used to illustrate JFET characteristics.

Key specifications include:

- N-channel JFET
- 40 V drain-source voltage rating
- Fully pinched off at approximately **VGS = -1.5 V**

 ![image](https://global.discourse-cdn.com/digikey/original/3X/6/b/6bfcb04938779a188df9d246003df17ae3a59a2c.png)

 ![image](https://global.discourse-cdn.com/digikey/original/3X/1/e/1e19fbea88728aa1f9fdb4be011aeb67c79f02e2.png)

The arrow in the N-channel JFET symbol indicates the direction that gate current would flow if gate current were present.

This condition should be avoided. In other words:

**The PN junction formed between the gate and the channel should never be forward-biased during normal operation.**

* * *

# Limitations of JFETs

The MMBFJ201 datasheet illustrates one common drawback of JFETs:

## Wide Parameter Variation

Parameters such as:

- Gate-source cutoff voltage (**VGS(off)**)
- Saturation drain current ( **IDSS** )

can vary significantly between devices and manufacturing lots.

* * *

# JFET Operating Regions

The output characteristics of a JFET can be divided into:

1. **Linear Region**
2. **Transition Region**
3. **Saturation Region (Constant Current Region)**

 ![image](https://global.discourse-cdn.com/digikey/original/3X/5/5/553938467d6658309380906513a79575a52771ae.jpeg)

If **VGS** becomes excessive, operation may enter the:

1. **Avalanche Breakdown Region**

where avalanche breakdown occurs across the PN junction.

Transfer characteristics also show that:

- At a fixed **VGS** ,
- Drain current ( **ID** ) generally increases as temperature rises.

* * *

# Design and Usage Considerations

Because N-channel devices use electrons as charge carriers:

- Electron mobility is higher.
- Switching and conduction characteristics are generally better.
- Manufacturing cost is typically lower.

For these reasons, **N-channel JFETs are usually preferred in practical designs**.

## 1. Avoid Forward-Biasing the Gate

- The gate-source PN junction normally operates under reverse bias.
- If the gate voltage exceeds approximately **0.6 V** ,
- The PN junction may become forward-biased.
- Excessive gate current may result.

## 2. Limit Gate Current

- Gate leakage current is typically in the nanoampere (nA) range.
- If forward bias cannot be avoided,
- A series current-limiting resistor should be used.
- A value of **100 kΩ or greater** is recommended.

## 3. Observe ESD Precautions

Although JFETs are more robust than MOSFETs with respect to electrostatic discharge, their extremely high input impedance still requires careful handling.

Recommended precautions include:

- Avoid repeatedly soldering the same device.
- Ensure operators are properly grounded.
- Short all three terminals together before soldering.
- Avoid repeated rework operations.
- Never leave the gate terminal floating during testing.