For questions regarding the cable length tolerance of the Omega RTD‑831‑MTP Bolt‑On RTD Sensor, we have verified this information with the manufacturer. Please see their response below.
Omega RTD probes are considered Commercial/ “COTS” parts. As such, many specs like this are not controlled.
The cable length is measured by hand by the Assembler. Normally they are within ½” of the desired length but it can vary from probe to probe.
Especially since some cable insulation on the cold end needs to be removed and stripped back, to install the male connector.
Also important to note that other cable lengths are available on this sensor. In both Inch and Meter units of measure if needed…
Applicable Part Numbers
| DigiKey Part Number | Manufacturer Part Number |
|---|---|
| 5880-RTD-831-MTP-ND | RTD-831-MTP |
| 5880-RTDM12-G1/8-3MM-24MM-A-ND | RTDM12-G1/8-3MM-24MM-A |
| 5880-RTD-831-SE-ND | RTD-831-SE |
| 5880-RTD-831-4M-SE-ND | RTD-831-4M-SE |
| 5880-RTD-809-ND | RTD-809 |
| 5880-RTD-860-ND | RTD-860 |