To power up the alarm, which is originally powered by a 3V lithium battery.
A 12V wall cube adaptor was repurposed for the main power supply. Therefore, a 12V to 6V buck converter was needed. Since there was a radio frequency link between the outside siren and the internal base station, this converter needed to be very low noise.
Figure 3. The 12V to 6V buck converter.
The LTM8063 provided the perfect solution. It is a self-contained converter, comprising the silicon, FETs, and inductor in a 6.25mm × 4mm package and can operate up to 40V with an output current of 2A.
The LTM8063 buck converter reduces the 12 V input from the wall adapter to approximately 6.1 V, matching the measured voltage of the original battery supply. It was selected for its low-noise performance, which is important because the exterior siren communicates with the internal base station through a radio frequency link.
Figure 4. The final prototype.
The switchover circuit and power supply were integrated into a single enclosure. The DC2494A (LTM8063 evaluation kit) was mounted on top, with two switchover boards installed underneath. A wall power adapter provided the primary power source, while CR123A batteries were used as backup power.
Related Topics:
What is the purpose of the backup battery system in a burglar alarm?
How does the backup battery system work when the mains power supply fails?
How does the switchover circuit prevent backup batteries from powering the system normally?
Applicable Part Numbers
LT4423AV#TRPBF
505-LT4423AV#TRPBFCT
505-LT4423AV#TRPBFTR-ND
505-LT4423AV#TRPBFCT-ND
505-LT4423AV#TRPBFDKR-ND
505-LT4423AV#TRPBFDKR
505-LT4423AV#TRPBFTR
505-DC2494A-ND
LTM8063EY#PBF
LTM8063IY