Hello @oliverp2003taylor1,
This is the Johari window question applied to microcontrollers. How do you reduce your blind spots and increase the arena size.
If you want a real challenge, tackle the bipolar stepper motor:
- You construct the drivers using discrete transistors or MOSFETs
- You implement the code using a time based ISR
- You interpret the real-time feedback when the timing slips and the motor stalls
- You increase speed by increasing voltage and PWM the motor drivers or use series resistors to reduce the time constant
As a final objective, construct the system so that the stepper motor will ramp up to full speed and then ramp down. This is necessary as a stepper motor cannot be instantaneously accelerated to full speed. It will stall if pushed too hard.
You will need to leave the comfort of the Arduino IDE for bare-metal programming of the microcontroller e.g., precise time control via an ISR.
I wish you every success. But be forewarned, this is not trivial. It will take the better part of a year to make the stepper motor sing like a slide whistle (this metaphor will reveal itself with time).
Success is slow and measured but, to an engineer, there is nothing more satisfying than success after months of struggle. You will know why it works and have a new definition of what make a microcontroller application solid.
Happy soldering,
APDahlen
P.S. The project I describe forces you to address the questions in your original post. The H-bridge required to drive the stepper is an essential building block for power electronics. Also, the stepper motor is absolutely dependent on timing.
That transition from ‘it works on my desk’ to ‘it works for a year in the field’ is a massive mindset shift.
For me, the biggest ‘level up’ moment was finally embracing Watchdog Timers (WDT) and State Machines. I used to rely on delay() and hope for the best, but as APDahlen pointed out, that’s just asking for a hang. Realizing that the hardware can (and should) recover itself from unexpected glitches was a game changer for my unattended projects.
I also take his point about the ‘physical’ side very seriously, moving from messy breadboard jumpers to soldered connections and proper power conditioning is often the difference between a project that lasts a week and one that lasts forever…. It’s those boring ‘industrial’ habits that actually make the fun stuff possible.
Hello @oliverp2003taylor1,
May I recommend material written by Michael J. Pont.
He has a unique way of looking at the microcontroller and associate hardware. He forces us to ask what is in control. Ref:
Patterns for Time-Triggered Embedded Systems | SafeTTy Systems Ltd
Sincerely,
Aaron
hey, thanks for this link. i’ll check it out.
1 Like