------Question for 2002187100 Please Put your question below------
The data sheet for MOLEX’s crimp tool 2002187100 states that the tool works with 22-26 AWG wire. That data sheet also states this tool is compatible with Molex MicroClasp female terminals, p/n 561349000 and 561349100, whose wire gauge range is 28-22 AWG.
https://www.molex.com/en-us/products/part-detail/2002187100?display=pdf
I want to confirm that this crimp tool will work with these particular female connectors when using 28 AWG stranded wire.
Hello,
I have checked on Molex’s website and have confirmed that this tool will also work with the MicroClasp terminals down to 28AWG wire.
1 Like
Thanks for checking on this for me, Rob.
FWIW, when I initially scanned the “parts detail” PDF file for that tool, I didn’t notice that the “Tooling Specifications” section has a link to another PDF file that provides more detailed information about that hand tool:
https://www.molex.com/content/dam/molex/molex-dot-com/products/automated/en-us/applicationtoolingspecificationpdf/200/200218/2002187100-000.pdf
A few moments ago I downloaded that PDF and scanned it. I that PDF’s SCOPE section there’s a table, and under that table is a note (#4) that says, “28 AWG wire is not recommended for use in this [56134-9x00] terminal. Use 22-26 AWG wire for better crimp quality.” So, it seems 28 AWG can be used, but it’s not recommended.