ZDS II - Z8 Encore! version 5.7.0 and the ZUSBESC0200ZACG

Does anyone have a copy of ZDS II - Z8 Encore! version 5.7.0 that I can have? The Zilog website appears to be a bit neglected and downloads of *.zip files are corrupt.

This topic is partly covered in the thread Z8FS040BSB20EG, but I was limited to 3 responses.

I purchased 2 ZUSBESC0200ZACG Z8 Encore USB programming interfaces that I’m unable to use. I have been using the previous USB smart cable for many years without issues. This is very different from the ZUSBESC0200ZACG. The old device runs with a 3 wire interface to the target device. By default, the ZUSBESC0200ZACG adds another two pins that appear to require handshaking with the target. I have seen a manual which depicts software with a menu item to disable this and am hoping that the ZDS II - Z8 Encore! version 5.7.0 has this feature, otherwise I’m stuck.

Problem solved. File downloaded from Zilog web correctly after many tries