U-Boot SPL 2019.04-dirty (Oct 17 2020 - 13:20:56 -0400) Trying to boot from MMC1 U-Boot 2019.04-dirty (Oct 17 2020 - 13:20:56 -0400) CPU : AM335X-GP rev 2.1 I2C: ready DRAM: 256 MiB No match for driver 'omap_hsmmc' No match for driver 'omap_hsmmc' Some drivers were not found Reset Source: Power-on reset has occurred. RTC 32KCLK Source: External. MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 Loading Environment from EXT4... ** File not found /boot/uboot.env ** ** Unable to read "/boot/uboot.env" from mmc0:1 ** not set. Validating first E-fuse MAC Net: eth0: RGMII MODE cpsw Press SPACE to abort autoboot in 5 seconds switch to partitions #0, OK mmc0 is current device SD/MMC found on device 0 switch to partitions #0, OK mmc0 is current device Scanning mmc 0:1... switch to partitions #0, OK mmc0 is current device gpio set 54 Checking for: /uEnv.txt ... Checking for: /boot.scr ... Checking for: /boot/boot.scr ... Checking for: /boot/uEnv.txt ... gpio set 55 2165 bytes read in 48 ms (43.9 KiB/s) Loaded environment from /boot/uEnv.txt testing DTB(ep11291.dtb) debug: [dtb=ep11291.dtb] ... Using: dtb=ep11291.dtb ... Checking if uname_r is set in /boot/uEnv.txt... gpio set 56 Running uname_boot ... loading /boot/vmlinuz-5.4.66EPN11291-ti-r18 ... 7270912 bytes read in 984 ms (7 MiB/s) setenv fdtdir /boot/dtbs/5.4.66EPN11291-ti-r18 ... debug: [enable_uboot_overlays=] ... loading /boot/ep11291.dtb ... 30463 bytes read in 54 ms (550.8 KiB/s) uboot_overlays: add [enable_uboot_overlays=1] to /boot/uEnv.txt to enable... debug: [console=ttyS0,115200n8 earlyprintk coherent_pool=1M net.ifnames=0 rng_core.default_quality=100 root=/dev/mmcblk0p1 ro rootfstype=ext4 rootwait coherent_pool=1M net.ifnames=0 rng_core.default_quality=100 systemd.unit=rescue.target] ... debug: [bootz 0x82000000 - 0x88000000] ... ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Loading Device Tree to 8df55000, end 8df5f6fe ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 5.4.66EPN11291-ti-r18 (rich@poseiden) (gcc version 8.3.0 (GNU Toolchain for the A-profile Architecture 8.3-2019.03 (arm-rel-8.36))) #1 PREEMPT Tue Oct 20 18:43:42 EDT 2020 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=50c5387d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] OF: fdt: Machine model: Flight Circuits EPN11291 [ 0.000000] Memory policy: Data cache writeback [ 0.000000] efi: Getting EFI parameters from FDT: [ 0.000000] efi: UEFI not found. [ 0.000000] cma: Reserved 48 MiB at 0x8a800000 [ 0.000000] CPU: All CPU(s) started in SVC mode. [ 0.000000] AM335X ES2.1 (neon) [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 64452 [ 0.000000] Kernel command line: console=ttyS0,115200n8 earlyprintk coherent_pool=1M net.ifnames=0 rng_core.default_quality=100 root=/dev/mmcblk0p1 ro rootfstype=ext4 rootwait coherent_pool=1M net.ifnames=0 rng_core.default_quality=100 systemd.unit=rescue.target [ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes, linear) [ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes, linear) [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off [ 0.000000] Memory: 194640K/260096K available (7168K kernel code, 934K rwdata, 2956K rodata, 1024K init, 297K bss, 16304K reserved, 49152K cma-reserved, 0K highmem) [ 0.000000] random: get_random_u32 called from __kmem_cache_create+0x2b/0x31c with crng_init=0 [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1 [ 0.000000] ftrace: allocating 35692 entries in 70 pages [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] Tasks RCU enabled. [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies. [ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16 [ 0.000000] IRQ: Found an INTC at 0x(ptrval) (revision 5.0) with 128 interrupts [ 0.000000] OMAP clockevent source: timer2 at 25000000 Hz [ 0.000028] sched_clock: 32 bits at 25MHz, resolution 40ns, wraps every 85899345900ns [ 0.000073] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 76450417870 ns [ 0.000102] OMAP clocksource: timer1 at 25000000 Hz [ 0.001521] timer_probe: no matching timers found [ 0.002043] Console: colour dummy device 80x30 [ 0.002178] Calibrating delay loop... 297.98 BogoMIPS (lpj=595968) [ 0.037789] pid_max: default: 32768 minimum: 301 [ 0.038621] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes, linear) [ 0.038664] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes, linear) [ 0.038925] *** VALIDATE tmpfs *** [ 0.040601] *** VALIDATE proc *** [ 0.041274] *** VALIDATE cgroup1 *** [ 0.041311] *** VALIDATE cgroup2 *** [ 0.041452] CPU: Testing write buffer coherency: ok [ 0.041573] CPU0: Spectre v2: using BPIALL workaround [ 0.043963] Setting up static identity map for 0x80100000 - 0x80100054 [ 0.044383] rcu: Hierarchical SRCU implementation. [ 0.049879] EFI services will not be available. [ 0.050909] devtmpfs: initialized [ 0.073451] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 0.074866] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns [ 0.074921] futex hash table entries: 256 (order: -1, 3072 bytes, linear) [ 0.083749] pinctrl core: initialized pinctrl subsystem [ 0.086684] NET: Registered protocol family 16 [ 0.096566] DMA: preallocated 1024 KiB pool for atomic coherent allocations [ 0.140320] l4_wkup_cm:clk:0010:0: failed to disable [ 0.143101] audit: initializing netlink subsys (disabled) [ 0.145385] cpuidle: using governor ladder [ 0.145478] cpuidle: using governor menu [ 0.149867] audit: type=2000 audit(0.136:1): state=initialized audit_enabled=0 res=1 [ 0.160174] platform 44e07000.gpio: Cannot lookup hwmod 'gpio1' [ 0.160546] omap_gpio 44e07000.gpio: Could not get gpio dbck. Disable debounce [ 0.160599] omap_gpio 44e07000.gpio: _od_fail_runtime_resume: FIXME: missing hwmod/omap_dev info [ 0.161537] OMAP GPIO hardware version 0.1 [ 0.162316] platform 4804c000.gpio: Cannot lookup hwmod 'gpio2' [ 0.162688] omap_gpio 4804c000.gpio: Could not get gpio dbck. Disable debounce [ 0.162735] omap_gpio 4804c000.gpio: _od_fail_runtime_resume: FIXME: missing hwmod/omap_dev info [ 0.164209] platform 481ac000.gpio: Cannot lookup hwmod 'gpio3' [ 0.164562] omap_gpio 481ac000.gpio: Could not get gpio dbck. Disable debounce [ 0.164607] omap_gpio 481ac000.gpio: _od_fail_runtime_resume: FIXME: missing hwmod/omap_dev info [ 0.166137] platform 481ae000.gpio: Cannot lookup hwmod 'gpio4' [ 0.166489] omap_gpio 481ae000.gpio: Could not get gpio dbck. Disable debounce [ 0.166533] omap_gpio 481ae000.gpio: _od_fail_runtime_resume: FIXME: missing hwmod/omap_dev info [ 0.167959] platform 44e09000.serial: Cannot lookup hwmod 'uart1' [ 0.168644] platform 48022000.serial: Cannot lookup hwmod 'uart2' [ 0.169605] platform 48060000.mmc: Cannot lookup hwmod 'mmc1' [ 0.170380] platform 481d8000.mmc: Cannot lookup hwmod 'mmc2' [ 0.178387] platform 4a100000.ethernet: Cannot lookup hwmod 'cpgmac0' [ 0.183130] hw-breakpoint: debug architecture 0x4 unsupported. [ 0.240539] debugfs: Directory '49000000.edma' with parent 'dmaengine' already present! [ 0.240605] edma 49000000.edma: TI EDMA DMA engine driver [ 0.247556] SCSI subsystem initialized [ 0.248948] pps_core: LinuxPPS API ver. 1 registered [ 0.248975] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti [ 0.250156] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400 [ 0.251673] Advanced Linux Sound Architecture Driver Initialized. [ 0.255006] clocksource: Switched to clocksource timer1 [ 1.027026] random: fast init done [ 2.625290] *** VALIDATE bpf *** [ 2.626148] VFS: Disk quotas dquot_6.6.0 [ 2.626328] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes) [ 2.626577] *** VALIDATE ramfs *** [ 2.652089] thermal_sys: Registered thermal governor 'fair_share' [ 2.652106] thermal_sys: Registered thermal governor 'bang_bang' [ 2.652143] thermal_sys: Registered thermal governor 'step_wise' [ 2.653103] NET: Registered protocol family 2 [ 2.655297] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 4096 bytes, linear) [ 2.655389] TCP established hash table entries: 2048 (order: 1, 8192 bytes, linear) [ 2.655471] TCP bind hash table entries: 2048 (order: 1, 8192 bytes, linear) [ 2.655545] TCP: Hash tables configured (established 2048 bind 2048) [ 2.655816] UDP hash table entries: 256 (order: 0, 4096 bytes, linear) [ 2.655873] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes, linear) [ 2.656409] NET: Registered protocol family 1 [ 2.658076] RPC: Registered named UNIX socket transport module. [ 2.658107] RPC: Registered udp transport module. [ 2.658127] RPC: Registered tcp transport module. [ 2.658146] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 2.658177] NET: Registered protocol family 44 [ 2.660444] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available [ 2.665081] Initialise system trusted keyrings [ 2.665637] workingset: timestamp_bits=14 max_order=16 bucket_order=2 [ 2.684215] zbud: loaded [ 2.691215] NFS: Registering the id_resolver key type [ 2.691299] Key type id_resolver registered [ 2.691323] Key type id_legacy registered [ 2.691372] nfs4filelayout_init: NFSv4 File Layout Driver Registering... [ 2.691982] fuse: init (API version 7.31) [ 2.692269] *** VALIDATE fuse *** [ 2.692304] *** VALIDATE fuse *** [ 2.807398] Key type asymmetric registered [ 2.807434] Asymmetric key parser 'x509' registered [ 2.807569] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 246) [ 2.808039] io scheduler mq-deadline registered [ 2.813306] pinctrl-single 44e10800.pinmux: 142 pins, size 568 [ 2.819527] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle [ 2.822490] Serial: 8250/16550 driver, 6 ports, IRQ sharing disabled [ 2.829482] omap8250 44e09000.serial: _od_fail_runtime_resume: FIXME: missing hwmod/omap_dev info [ 2.830220] printk: console [ttyS0] disabled [ 2.830441] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 30, base_baud = 3000000) is a 8250 [ 3.600551] printk: console [ttyS0] enabled [ 3.606531] omap8250 48022000.serial: _od_fail_runtime_resume: FIXME: missing hwmod/omap_dev info [ 3.616273] 48022000.serial: ttyS1 at MMIO 0x48022000 (irq = 31, base_baud = 3000000) is a 8250 [ 3.629975] omap_rng 48310000.rng: Random Number Generator ver. 20 [ 3.636800] random: crng init done [ 3.642199] sdhci: Secure Digital Host Controller Interface driver [ 3.648514] sdhci: Copyright(c) Pierre Ossman [ 3.653857] omap_gpio 4804c000.gpio: Could not set line 27 debounce to 200000 microseconds (-524) [ 3.662875] omap_hsmmc 48060000.mmc: Got CD GPIO [ 3.667971] omap_hsmmc: probe of 48060000.mmc failed with error -2 [ 3.675081] omap_hsmmc: probe of 481d8000.mmc failed with error -2 [ 3.681664] sdhci-pltfm: SDHCI platform and OF driver helper [ 3.700832] libphy: Fixed MDIO Bus: probed [ 3.709577] cpsw 4a100000.ethernet: _od_fail_runtime_resume: FIXME: missing hwmod/omap_dev info [ 3.723490] omap_rtc 44e3e000.rtc: registered as rtc0 [ 3.729147] i2c /dev entries driver [ 3.736401] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec [ 3.744194] softdog: initialized. soft_noboot=0 soft_margin=60 sec soft_panic=0 (nowayout=0) [ 3.755965] cpufreq: cpufreq_online: CPU0: Running at unlisted freq: 600000 KHz [ 3.763638] cpu cpu0: dev_pm_opp_set_rate: failed to find current OPP for freq 600000000 (-34) [ 3.772526] cpufreq: cpufreq_online: CPU0: Unlisted initial frequency changed to: 300000 KHz [ 3.783160] ledtrig-cpu: registered to indicate activity on CPUs [ 3.790612] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2 [ 3.797470] omap-aes 53500000.aes: will run requests pump with realtime priority [ 3.812710] omap-sham 53100000.sham: hw accel on OMAP rev 4.3 [ 3.834282] remoteproc remoteproc0: wkup_m3 is available [ 3.857094] drop_monitor: Initializing network drop monitor service [ 3.864123] wireguard: WireGuard 0.0.20191219 loaded. See www.wireguard.com for information. [ 3.872770] wireguard: Copyright (C) 2015-2019 Jason A. Donenfeld . All Rights Reserved. [ 3.886945] NET: Registered protocol family 10 [ 3.904866] Segment Routing with IPv6 [ 3.909729] mip6: Mobile IPv6 [ 3.913492] NET: Registered protocol family 17 [ 3.919508] Key type dns_resolver registered [ 3.924200] mpls_gso: MPLS GSO support [ 3.929727] ThumbEE CPU extension supported. [ 3.934300] omap_voltage_late_init: Voltage driver support not added [ 3.941694] PM: Cannot get wkup_m3_ipc handle [ 3.948369] registered taskstats version 1 [ 3.952679] Loading compiled-in X.509 certificates [ 3.958006] zswap: loaded using pool lzo/zbud [ 3.965064] Key type ._fscrypt registered [ 3.969297] Key type .fscrypt registered [ 4.056975] PM: Cannot get wkup_m3_ipc handle [ 4.061665] remoteproc remoteproc0: powering up wkup_m3 [ 4.067963] PM: Cannot get wkup_m3_ipc handle [ 4.072608] remoteproc remoteproc0: Booting fw image am335x-pm-firmware.elf, size 217168 [ 4.083480] omap_rtc 44e3e000.rtc: setting system clock to 2000-01-01T00:00:00 UTC (946684800) [ 4.092826] wkup_m3_ipc 44e11324.wkup_m3_ipc: CM3 Firmware Version = 0x193