U-Boot SPL 2018.01-rc3-00002-gb3322413b6 (Jan 02 2018 - 12:26:25) Trying to boot from MMC2 U-Boot 2018.01-rc3-00002-gb3322413b6 (Jan 02 2018 - 12:26:25 -0600), Build: jenkins-github_Bootloader-Builder-23 CPU : AM335X-GP rev 2.0 I2C: ready DRAM: 512 MiB No match for driver 'omap_hsmmc' No match for driver 'omap_hsmmc' Some drivers were not found Reset Source: Global external warm reset has occurred. Reset Source: Power-on reset has occurred. MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 Using default environment Board: BeagleBone Black not set. Validating first E-fuse MAC BeagleBone Black: BeagleBone: cape eeprom: i2c_probe: 0x54: BeagleBone: cape eeprom: i2c_probe: 0x55: BeagleBone: cape eeprom: i2c_probe: 0x56: BeagleBone: cape eeprom: i2c_probe: 0x57: Net: eth0: MII MODE cpsw, usb_ether Press SPACE to abort autoboot in 2 seconds board_name=[A335BNLT] ... board_rev=[0A5C] ... Card did not respond to voltage select! mmc_init: -95, time 13 Card did not respond to voltage select! mmc_init: -95, time 12 Card did not respond to voltage select! mmc_init: -95, time 13 gpio: pin 56 (gpio 56) value is 0 gpio: pin 55 (gpio 55) value is 0 gpio: pin 54 (gpio 54) value is 0 gpio: pin 53 (gpio 53) value is 1 Card did not respond to voltage select! mmc_init: -95, time 13 Card did not respond to voltage select! mmc_init: -95, time 13 switch to partitions #0, OK mmc1(part 0) is current device Scanning mmc 1:1... gpio: pin 56 (gpio 56) value is 0 gpio: pin 55 (gpio 55) value is 0 gpio: pin 54 (gpio 54) value is 0 gpio: pin 53 (gpio 53) value is 1 switch to partitions #0, OK mmc1(part 0) is current device gpio: pin 54 (gpio 54) value is 1 Checking for: /uEnv.txt ... Checking for: /boot.scr ... Checking for: /boot/boot.scr ... Checking for: /boot/uEnv.txt ... gpio: pin 55 (gpio 55) value is 1 2044 bytes read in 52 ms (38.1 KiB/s) Loaded environment from /boot/uEnv.txt Checking if uname_r is set in /boot/uEnv.txt... gpio: pin 56 (gpio 56) value is 1 Running uname_boot ... loading /boot/vmlinuz-4.9.74-ti-r90 ... 9951976 bytes read in 674 ms (14.1 MiB/s) uboot_overlays: [uboot_base_dtb=am335x-boneblack-uboot.dtb] ... uboot_overlays: Switching too: dtb=am335x-boneblack-uboot.dtb ... loading /boot/dtbs/4.9.74-ti-r90/am335x-boneblack-uboot.dtb ... 61174 bytes read in 77 ms (775.4 KiB/s) uboot_overlays: [fdt_buffer=0x60000] ... uboot_overlays: loading /lib/firmware/AM335X-20-00A0.dtbo ... 537 bytes read in 779 ms (0 Bytes/s) uboot_overlays: loading /lib/firmware/BB-BONE-eMMC1-01-00A0.dtbo ... 1584 bytes read in 932 ms (1000 Bytes/s) uboot_overlays: loading /lib/firmware/BB-HDMI-TDA998x-00A0.dtbo ... 4915 bytes read in 506 ms (8.8 KiB/s) uboot_overlays: loading /lib/firmware/BB-ADC-00A0.dtbo ... 867 bytes read in 451 ms (1000 Bytes/s) uboot_overlays: loading /lib/firmware/AM335X-PRU-UIO-00A0.dtbo ... 1013 bytes read in 1173 ms (0 Bytes/s) uboot_overlays: unable to find [mmc 1:1 /lib/firmware/univ-bbb-EVA-00A0.dtbo]... loading /boot/initrd.img-4.9.74-ti-r90 ... 5588082 bytes read in 428 ms (12.5 MiB/s) debug: [console=ttyO0,115200n8 root=/dev/mmcblk1p1 ro rootfstype=ext4 rootwait coherent_pool=1M net.ifnames=0 quiet] ... debug: [bootz 0x82000000 0x88080000:554472 88000000] ... ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Loading Ramdisk to 8faab000, end 8ffff472 ... OK reserving fdt memory region: addr=88000000 size=71000 Loading Device Tree to 8fa37000, end 8faaafff ... OK Starting kernel ... [ 0.000987] clocksource_probe: no matching clocksources found [ 1.320790] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle [ 1.495529] omap_hsmmc 481d8000.mmc: prop pinctrl-0 index 0 invalid phandle [ 1.529924] omap_voltage_late_init: Voltage driver support not added [ 1.537079] PM: Cannot get wkup_m3_ipc handle [ 1.935996] bone_capemgr bone_capemgr: slot #0: No cape found [ 1.967025] bone_capemgr bone_capemgr: slot #1: No cape found [ 1.999692] bone_capemgr bone_capemgr: slot #2: No cape found [ 2.032335] bone_capemgr bone_capemgr: slot #3: No cape found [ 2.047949] musb-hdrc musb-hdrc.1: VBUS_ERROR in a_wait_vrise (88,