3000W 12V DC power supply rig

Thanks, that answers all of my questions except one last concern,

I think I will go with one of my two 240V outlets that I realize can each provide 30A and 40A. Since the power supply ET3200-12-069RA from digikey has a 17A maximum limit, am I not allowed to just plug in this power supply directly to my 240V outlet? I would assume that the power supply will only draw 13A since at 240V this is the current required to produce the 3000W output. Is there any reason why the power supply might draw more than this or more than the 17A limit once I plug it in directly to my 240V outlet? Is there any intermediary device needed to limit the current supplied from the outlet to the power supply or should the power supply automatically draw the required current safely to obtain it’s rated power of 3000W on it’s own?

Thank you