Anyone can locate JOC341

does anyone knows where i can find this part JOC341?

Hello,
Welcome to the DigiKey TechForum. This isn’t a part listed in our system , I did check and was unsuccessful in finding an alternate to offer for it. If you perform a Google search on part JOC341 you should see some options where this part is available.

Hi DemiGod,

If you have trouble finding that part, here are some similar parts from Toshiba’s TLP5754 and TLP5774 series which are quite similar to various versions of the JOC341 in terms of both electrical and physical specifications.

Please verify whether they would be suitable alternatives in your particular application.

good evening David, is the ACPL-W341-500E the same thing here. Let me know if it can work also.

Hello,

I think David is out until tomorrow and should get back.

I do see there are 2 versions that are stocking of that part and added the 500E and 560E to this link.

Isolators | Isolators - Gate Drivers | DigiKey

Thank you
Ryan

Hi DemiGod,

The ACPL-W341-500E is also quite similar, though slightly slower in rise, fall, and propagation delay specs than the TLP5754, which is itself slightly slower than the JOC341. See respective datasheets for comparisons.

The reason I specifically mentioned the TLP5754 series previously was because it was the closest that I could find to matching the switching times of the JOC341. However, it is probably no coincidence that the JOC341 and the ACPL-W341-500E both have “341” in their respective part numbers. It’s highly likely that the JOC341 was modeled after the ACPL-W341-500E.

I would expect that in the vast majority of applications, either the TLP5754 or the ACPL-W341-500E would be quite suitable as alternatives, but I can not make that determination for you, as every application is unique and the one implementing the design must make the final determination.