Bistable relay 24vdc din rail

I’m looking for a 24vdc bistable relay, din rail, 1 module for light control, 220v 10a max load. If possible, a low-absorption coil (but it’s not essential)

Hello,
Welcome to our community and thank you for using our forum.
These are the two relays we carry in that series for 24V

Here is a DIN rail latching relay rated for 16A continuous:

Note that it is an “impulse” type, which means that each time voltage is applied to the “coil” it changes states between open and closed. Duration of impulse should be between 0.1s and 1hr.