Hi everyone,
I’m trying to build a Debian 12 with Linux kernel 6.1.y for my BeagleBoard-X15 (AM5728), and I want to enable OpenCL support (using TI’s OpenCL runtime).
What I’ve done so far:
- Followed a previous [Digi-Key Getting Started guide]Debian: Getting Started with the BeagleBoard-X15, which helped me boot Debian successfully.
- Successfully built and booted the system, but OpenCL does not work or fails to detect DSP/EVE devices.
- I have limited experience with kernel configurations, device trees, and OpenCL runtime setup.
My Goal:
To get OpenCL working (on the DSPs, like C66x) on Debian 12 with Linux 6.1.y kernel.
What I need help with:
- Kernel config: What specific config options are required to support OpenCL (e.g., TI-specific drivers or RPMsg support)?
- Device tree changes: Do I need to enable or modify anything to allow DSP/EVE access from Linux?
- OpenCL runtime: Do I need to install or rebuild any userspace OpenCL packages from TI?
- Validation: How do I check that OpenCL detects the DSPs (e.g.,
clinfo,dsplib_fft, etc.)?
Any clear guidance, or updated step-by-step for Debian 12 + kernel 6.1 + OpenCL on BB-X15 would be very helpful!
Thanks in advance!
– Tamilselvan