Capacitor k5u 104m

I would like the good specs or an alternative digikey for that ceramic capacitor k5u 104m

Thank you,

Hello,
Welcome to the DigiKey TechForum antoue.

As per ordering information from Kemet below. This looks to be 0.1uF 50V 20% through hole capacitor.

399-9842-ND seems it would be a decent alternate. Its slightly better in tolerance at 10% and it has a X7R rating which is also a bit better than the general purpose Z5U.

Hope that helps. Have a great day.