Conductive epoxy volume

Conductive Epoxy AA-DUCT-902-1 is a suitable option for my project, however, the associated volume is not provided on the data sheet.

A value for the volume, or guidance on where this information could be found would be appreciated.

Hello a1885260,

Welcome to the DigiKey TechForum.

Seems the AA-DUCT-902-1 that ends in that -1 suffix would be the 1.5g pouch. The AA-DUCT-902-2 is also offered on our website and that looks to be the 2.5g pouch. This from their pricetable on these: AA-DUCT 902 Silver Epoxy Adhesive, Electrically Conductive, Room Temp Curing, Air Dr