CTSは、品番194-8MSTを含むDIPスイッチのシリーズを提供しています。このスイッチは、194-8MSTNのように「N」のサフィックスが付いた形で、どこか他でも目にしたことがあるかもしれません。この「N」サフィックスは部品に影響しますか?また、DigiKeyのNなし品番のスイッチは「N」ありのものと互換性があるでしょうか?
もちろん互換性があります。スイッチ自体はどちらの品番でも同一ですが、末尾の「N」は、デバイスが「OFF」ではなく「ON」に設定された状態で出荷されることを示しています。組み立て工程でこのデフォルト出荷位置を考慮しない場合、またはそれに適応できる場合、この2つの品番の部品は完全に交換が可能です。