Current handling on Keystone 1043P holder

What is the maximum current-handling capacity on the Keystone 1043P Li-Ion battery holder?

Hi bri4eng,

This holder is meant for 1 cell of 18650 battery cell size so based on that, since 1 cell of that battery can produce 3.5Ah or 3500mAh it is safe to assume that the holder can handle 3.5A of current. I found this to be the max amps one cell of this battery size can produce but most of them are at 2.6Ah or 2600mAh.

But there are no specific designations in any documentation of this holder, such as manufacturers website or even the data sheet, of what the maximum current these are rated for is. Hope that helps.

Maybe someone else might have some more insight on this.

2 Likes