There is a mismatch in an OEM datasheet.
MFR: Cal Test Electronics
MFR Part Number: CT2244-0
On DigiKey, the part number CT2244-# has a solder hole. And CT2911-# has a Faston termination. But in the datasheet, the descriptions don’t match the diagrams they are associated with.
I can figure out which is which, but I wont ever be 100% sure which one is correct until I receive the order. Because I also know that the pictures on DigiKey can be incorrect too. I can confidently say that the OEM Datasheet is incorrect, but what I cant be confident in is if DigiKey corrected that when they added them to the catalog. I don’t want to assume, and then get the wrong part.
/https://mm.digikey.com/Volume0/opasdata/d220001/medias/docus/4846/DS_1768_Catalog.pdf
page 61