Availability
Boards:
- MCIMX8M-EVKB at Digi-Key
- MCIMX8M-EVK (Obsolete) at Digi-Key
Vendor Documentation
- NXP Documentation: https://www.nxp.com
- Board Documentation: https://www.nxp.com/part/MCIMX8M-EVKB#/
Notes
Jumpers 1100 (microSD)
Basic Requirements
- Running a recent supported release of Debian, Fedora or Ubuntu on a x86 64bit based PC; without OS Virtualization Software.
- Many of the listed commands assume /bin/bash as the default shell.
- ARM Cross Compiler – Linaro: https://www.linaro.org
- Linaro Toolchain Binaries: https://www.linaro.org/downloads/
- Bootloader
- Das U-Boot – the Universal Boot Loader: http://www.denx.de/wiki/U-Boot
- Source: https://github.com/u-boot/u-boot/
- Linux Kernel
- Linus’s Mainline tree: https://git.kernel.org/pub/scm/linux/kernel/git/torvalds/linux.git
- ARM based rootfs
- Debian: https://www.debian.org
- Ubuntu: https://www.ubuntu.com
ARM Cross Compiler: GCC
This is a pre-built (64bit) version of GCC that runs on generic linux, sorry (32bit) x86 users, it’s time to upgrade…
Download/Extract:
#user@localhost:~$
wget -c https://developer.arm.com/-/media/Files/downloads/gnu-a/8.3-2019.03/binrel/gcc-arm-8.3-2019.03-x86_64-aarch64-linux-gnu.tar.xz
tar xf gcc-arm-8.3-2019.03-x86_64-aarch64-linux-gnu.tar.xz
export CC=`pwd`/gcc-arm-8.3-2019.03-x86_64-aarch64-linux-gnu/bin/aarch64-linux-gnu-
Test Cross Compiler:
#user@localhost:~$
${CC}gcc --version
#Test Output:
aarch64-linux-gnu-gcc (GNU Toolchain for the A-profile Architecture 8.3-2019.03 (arm-rel-8.36)) 8.3.0
Copyright (C) 2018 Free Software Foundation, Inc.
This is free software; see the source for copying conditions. There is NO
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
Linux Kernel
This script will build the kernel, modules, device tree binaries and copy them to the deploy directory.
Download:
#user@localhost:~$
git clone https://github.com/RobertCNelson/imx8-linux-dev
cd imx8-linux-dev/
For v5.4.x (Longterm 5.4.x):
#user@localhost:~/imx8-linux-dev$
git checkout origin/v5.4.x -b tmp
Build:
#user@localhost:~/imx8-linux-dev$
./build_kernel.sh
Root File System
Debian 10
| User | Password |
|---|---|
| debian | temppwd |
| root | root |
Download:
#user@localhost:~$
wget -c https://rcn-ee.com/rootfs/eewiki/minfs/debian-10.9-minimal-arm64-2021-04-14.tar.xz
Verify:
#user@localhost:~$
sha256sum debian-10.9-minimal-arm64-2021-04-14.tar.xz
#sha256sum output:
bad3637300734571c2a17e84ba68d47698624c4de62fce44819dfe79a684e97c debian-10.9-minimal-arm64-2021-04-14.tar.xz
Extract:
#user@localhost:~$
tar xf debian-10.9-minimal-arm64-2021-04-14.tar.xz
Setup microSD card
We need to access the External Drive to be utilized by the target device. Run lsblk to help figure out what linux device has been reserved for your External Drive.
#Example: for DISK=/dev/sdX
lsblk
NAME MAJ:MIN RM SIZE RO TYPE MOUNTPOINT
sda 8:0 0 465.8G 0 disk
├─sda1 8:1 0 512M 0 part /boot/efi
└─sda2 8:2 0 465.3G 0 part / <- Development Machine Root Partition
sdb 8:16 1 962M 0 disk <- microSD/USB Storage Device
└─sdb1 8:17 1 961M 0 part <- microSD/USB Storage Partition
#Thus you would use:
export DISK=/dev/sdb
#Example: for DISK=/dev/mmcblkX
lsblk
NAME MAJ:MIN RM SIZE RO TYPE MOUNTPOINT
sda 8:0 0 465.8G 0 disk
├─sda1 8:1 0 512M 0 part /boot/efi
└─sda2 8:2 0 465.3G 0 part / <- Development Machine Root Partition
mmcblk0 179:0 0 962M 0 disk <- microSD/USB Storage Device
└─mmcblk0p1 179:1 0 961M 0 part <- microSD/USB Storage Partition
#Thus you would use:
export DISK=/dev/mmcblk0
Erase partition table/labels on microSD card:
sudo dd if=/dev/zero of=${DISK} bs=1M count=100
Install Bootloader:
#user@localhost:~$
wget -c https://github.com/eewiki/u-boot-builds/raw/main/imx8mqevk/2021.02.x/imx8-boot-sd.bin
sudo dd if=./imx8-boot-sd.bin of=${DISK} seek=33 bs=1k
Create Partition Layout:
With util-linux v2.26, sfdisk was rewritten and is now based on libfdisk.
#Check the version of sfdisk installed on your pc
sudo sfdisk --version
#Example Output
sfdisk from util-linux 2.27.1
#sfdisk >= 2.26.x
sudo sfdisk ${DISK} <<-__EOF__
8M,64M,0xc,*
65M,,,-
__EOF__
#sfdisk <= 2.25.x
sudo sfdisk --unit M ${DISK} <<-__EOF__
8,64,0xc,*
65,,,-
__EOF__
Format Partition:
for: DISK=/dev/mmcblkX
sudo mkfs.vfat -F 16 -n BOOT ${DISK}p1
sudo mkfs.ext4 -L rootfs ${DISK}p2
for: DISK=/dev/sdX
sudo mkfs.vfat -F 16 -n BOOT ${DISK}1
sudo mkfs.ext4 -L rootfs ${DISK}2
Mount Partition:
On most systems these partitions may be auto-mounted…
sudo mkdir -p /media/boot/
sudo mkdir -p /media/rootfs/
for: DISK=/dev/mmcblkX
sudo mount ${DISK}p1 /media/boot/
sudo mount ${DISK}p2 /media/rootfs/
for: DISK=/dev/sdX
sudo mount ${DISK}1 /media/boot/
sudo mount ${DISK}2 /media/rootfs/
Install Kernel and Root File System
To help new users, since the kernel version can change on a daily basis. The kernel building scripts listed on this page will now give you a hint of what kernel version was built.
-----------------------------
Script Complete
eewiki.net: [user@localhost:~$ export kernel_version=5.X.Y-Z]
-----------------------------
Copy and paste that “export kernel_version=5.X.Y-Z” exactly as shown in your own build/desktop environment and hit enter to create an environment variable to be used later.
export kernel_version=5.X.Y-Z
Copy Root File System
#user@localhost:~$
sudo tar xfvp ./debian-*-*-arm64-*/arm64-rootfs-*.tar -C /media/rootfs/
sync
sudo chown root:root /media/rootfs/
sudo chmod 755 /media/rootfs/
Copy Kernel Image
Kernel Image:
#user@localhost:~$
sudo cp -v ./imx8-linux-dev/deploy/${kernel_version}.Image /media/boot/Image
Copy Kernel Device Tree Binaries
#user@localhost:~$
sudo mkdir -p /media/boot/dtbs/
sudo tar xfvo ./imx8-linux-dev/deploy/${kernel_version}-dtbs.tar.gz -C /media/boot/dtbs/
sudo cp -v /media/boot/dtbs/freescale/imx8mq-evk.dtb /media/boot/imx8mq-evk.dtb
Copy Kernel Modules
#user@localhost:~$
sudo tar xfv ./imx8-linux-dev/deploy/${kernel_version}-modules.tar.gz -C /media/rootfs/
File Systems Table (/etc/fstab)
#user@localhost:~/$
sudo sh -c "echo '/dev/mmcblk1p2 / auto errors=remount-ro 0 1' >> /media/rootfs/etc/fstab"
sudo sh -c "echo '/dev/mmcblk1p1 /boot/uboot auto defaults 0 2' >> /media/rootfs/etc/fstab"
Remove microSD/SD card
sync
sudo umount /media/boot
sudo umount /media/rootfs
Comments
Any questions or comments please go to our TechForum: TechForum