This is a page about Octavo System’s TI Cortex-A8 based; OSD3358-SM-RED.
Availability
Boards:
- OSD3358-SM-RED at Digi-Key
Cables:
- (USB to serial adapter) TTL-232R-3V3 at Digi-Key
Basic Requirements
- Running a recent supported release of Debian, Fedora or Ubuntu on a x86 64bit based PC; without OS Virtualization Software.
- Many of the listed commands assume /bin/bash as the default shell.
- Kernel.org Cross Compilers – https://mirrors.edge.kernel.org/pub/tools/crosstool/
- Bootloader
- Das U-Boot – the Universal Boot Loader: http://www.denx.de/wiki/U-Boot
- Source: https://github.com/u-boot/u-boot/
- Linux Kernel
- Linus’s Mainline tree: https://git.kernel.org/pub/scm/linux/kernel/git/torvalds/linux.git
- ARM based rootfs
- Debian: https://www.debian.org
ARM Cross Compiler: GCC
This is a pre-built (64bit) version of GCC that runs on generic linux, sorry (32bit) x86 users, it’s time to upgrade…
Download/Extract:
#user@localhost:~$
wget -c https://mirrors.edge.kernel.org/pub/tools/crosstool/files/bin/x86_64/11.1.0/x86_64-gcc-11.1.0-nolibc-arm-linux-gnueabi.tar.xz
tar -xf x86_64-gcc-11.1.0-nolibc-arm-linux-gnueabi.tar.xz
export CC=`pwd`/gcc-11.1.0-nolibc/arm-linux-gnueabi/bin/arm-linux-gnueabi-
Test Cross Compiler:
#user@localhost:~$
${CC}gcc --version
#Test Output:
arm-linux-gnueabi-gcc (GCC) 11.1.0
Copyright (C) 2021 Free Software Foundation, Inc.
This is free software; see the source for copying conditions. There is NO
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
Bootloader: U-Boot
Das U-Boot – the Universal Boot Loader: http://www.denx.de/wiki/U-Boot
Depending on your Linux Distrubution, you will also need a host gcc and other tools, so with Debian/Ubuntu start with installing the build-essential meta package.
Download:
#user@localhost:~$
git clone -b v2022.04 https://github.com/u-boot/u-boot --depth=1
cd u-boot/
Patches:
#user@localhost:~/u-boot$
git pull --no-edit https://git.beagleboard.org/beagleboard/u-boot.git v2022.04-bbb.io-am335x-am57xx
Configure and Build:
#user@localhost:~/u-boot$
make ARCH=arm CROSS_COMPILE=${CC} distclean
make ARCH=arm CROSS_COMPILE=${CC} am335x_evm_defconfig
make ARCH=arm CROSS_COMPILE=${CC}
Linux Kernel
This script will build the kernel, modules, device tree binaries and copy them to the deploy directory.
Mainline
Download:
#~/
git clone https://github.com/RobertCNelson/bb-kernel ./kernelbuildscripts
cd kernelbuildscripts/
For am33x-v5.4 (Longterm 5.4.x):
#user@localhost:~/kernelbuildscripts$
git checkout origin/am33x-v5.4 -b tmp
For am33x-rt-v5.4 (Longterm 5.4.x + Real-Time Linux):
#user@localhost:~/kernelbuildscripts$
git checkout origin/am33x-rt-v5.4 -b tmp
For am33x-v5.10 (Longterm 5.10.x):
#user@localhost:~/kernelbuildscripts$
git checkout origin/am33x-v5.10 -b tmp
For am33x-rt-v5.10 (Longterm 5.10.x + Real-Time Linux):
#user@localhost:~/kernelbuildscripts$
git checkout origin/am33x-rt-v5.10 -b tmp
For am33x-v5.15 (Longterm 5.15.x):
#user@localhost:~/kernelbuildscripts$
git checkout origin/am33x-v5.15 -b tmp
For am33x-rt-v5.15 (Longterm 5.15.x + Real-Time Linux):
#user@localhost:~/kernelbuildscripts$
git checkout origin/am33x-rt-v5.15 -b tmp
Build:
#user@localhost:~/kernelbuildscripts$
./build_kernel.sh
TI BSP
Download:
#~/
git clone https://github.com/RobertCNelson/ti-linux-kernel-dev ./kernelbuildscripts
cd kernelbuildscripts/
For TI v5.4.x:
#~/kernelbuildscripts/
git checkout origin/ti-linux-5.4.y -b tmp
For TI v5.4.x: Real-Time
#~/kernelbuildscripts/
git checkout origin/ti-linux-rt-5.4.y -b tmp
For TI v5.10.x:
#~/kernelbuildscripts/
git checkout origin/ti-linux-5.10.y -b tmp
For TI v5.10.x: Real-Time
#~/kernelbuildscripts/
git checkout origin/ti-linux-rt-5.10.y -b tmp
Build:
#user@localhost:~/kernelbuildscripts$
./build_kernel.sh
Root File System
Debian 11
User | Password |
---|---|
debian | temppwd |
root | root |
Download:
#user@localhost:~$
wget -c https://rcn-ee.com/rootfs/eewiki/minfs/debian-11.3-minimal-armhf-2022-04-15.tar.xz
Verify:
#user@localhost:~$
sha256sum debian-11.3-minimal-armhf-2022-04-15.tar.xz
#sha256sum output:
575738843651de2962f251447f4742d4f33313d6f7f5edf282a401207f5e6646 debian-11.3-minimal-armhf-2022-04-15.tar.xz
Extract:
#user@localhost:~$
tar xf debian-11.3-minimal-armhf-2022-04-15.tar.xz
Setup microSD card
We need to access the External Drive to be utilized by the target device. Run lsblk to help figure out what linux device has been reserved for your External Drive.
#Example: for DISK=/dev/sdX
lsblk
NAME MAJ:MIN RM SIZE RO TYPE MOUNTPOINT
sda 8:0 0 465.8G 0 disk
├─sda1 8:1 0 512M 0 part /boot/efi
└─sda2 8:2 0 465.3G 0 part / <- Development Machine Root Partition
sdb 8:16 1 962M 0 disk <- microSD/USB Storage Device
└─sdb1 8:17 1 961M 0 part <- microSD/USB Storage Partition
#Thus you would use:
export DISK=/dev/sdb
#Example: for DISK=/dev/mmcblkX
lsblk
NAME MAJ:MIN RM SIZE RO TYPE MOUNTPOINT
sda 8:0 0 465.8G 0 disk
├─sda1 8:1 0 512M 0 part /boot/efi
└─sda2 8:2 0 465.3G 0 part / <- Development Machine Root Partition
mmcblk0 179:0 0 962M 0 disk <- microSD/USB Storage Device
└─mmcblk0p1 179:1 0 961M 0 part <- microSD/USB Storage Partition
#Thus you would use:
export DISK=/dev/mmcblk0
Erase partition table/labels on microSD card:
sudo dd if=/dev/zero of=${DISK} bs=1M count=10
Install Bootloader:
#user@localhost:~$
sudo dd if=./u-boot/MLO of=${DISK} count=2 seek=1 bs=128k
sudo dd if=./u-boot/u-boot-dtb.img of=${DISK} count=4 seek=1 bs=384k
Create Partition Layout:
With util-linux v2.26, sfdisk was rewritten and is now based on libfdisk.
#Check the version of sfdisk installed on your pc is atleast 2.26.x or newer.
sudo sfdisk --version
#Example Output
sfdisk from util-linux 2.27.1
#sfdisk >= 2.26.x
sudo sfdisk ${DISK} <<-__EOF__
4M,,L,*
__EOF__
Format Partition:
for: DISK=/dev/mmcblkX
sudo mkfs.ext4 -L rootfs ${DISK}p1
for: DISK=/dev/sdX
sudo mkfs.ext4 -L rootfs ${DISK}1
Mount Partition:
On most systems these partitions may be auto-mounted…
sudo mkdir -p /media/rootfs/
for: DISK=/dev/mmcblkX
sudo mount ${DISK}p1 /media/rootfs/
for: DISK=/dev/sdX
sudo mount ${DISK}1 /media/rootfs/
Backup Bootloader
This version of MLO/u-boot.img will be used on the “eMMC” flasher script on this page.
#~/
sudo mkdir -p /media/rootfs/opt/backup/uboot/
sudo cp -v ./u-boot/MLO /media/rootfs/opt/backup/uboot/
sudo cp -v ./u-boot/u-boot-dtb.img /media/rootfs/opt/backup/uboot/
Install Kernel and Root File System
To help new users, since the kernel version can change on a daily basis. The kernel building scripts listed on this page will now give you a hint of what kernel version was built.
-----------------------------
Script Complete
eewiki.net: [user@localhost:~$ export kernel_version=5.X.Y-Z]
-----------------------------
Copy and paste that “export kernel_version=5.X.Y-Z” exactly as shown in your own build/desktop environment and hit enter to create an environment variable to be used later.
export kernel_version=5.X.Y-Z
Copy Root File System
#Debian; Root File System: user@localhost:~$
sudo tar xfvp ./debian-*-*-armhf-*/armhf-rootfs-*.tar -C /media/rootfs/
sync
Set uname_r in /boot/uEnv.txt
#user@localhost:~$
sudo sh -c "echo 'uname_r=${kernel_version}' >> /media/rootfs/boot/uEnv.txt"
Copy Kernel Image
Kernel Image:
#user@localhost:~$
sudo cp -v ./kernelbuildscripts/deploy/${kernel_version}.zImage /media/rootfs/boot/vmlinuz-${kernel_version}
Copy Kernel Device Tree Binaries
#user@localhost:~$
sudo mkdir -p /media/rootfs/boot/dtbs/${kernel_version}/
sudo tar xfv ./kernelbuildscripts/deploy/${kernel_version}-dtbs.tar.gz -C /media/rootfs/boot/dtbs/${kernel_version}/
Copy Kernel Modules
#user@localhost:~$
sudo tar xfv ./kernelbuildscripts/deploy/${kernel_version}-modules.tar.gz -C /media/rootfs/
File Systems Table (/etc/fstab)
#user@localhost:~/$
sudo sh -c "echo '/dev/mmcblk0p1 / auto errors=remount-ro 0 1' >> /media/rootfs/etc/fstab"
Networking
Edit: /etc/network/interfaces
sudo nano /media/rootfs/etc/network/interfaces
Add:
#/etc/network/interfaces
auto lo
iface lo inet loopback
auto eth0
iface eth0 inet dhcp
Remove microSD/SD card
sync
sudo umount /media/rootfs
HDMI
This sections assumes you have already installed your favorite xorg based window manager, such as lxde, xfce, kde, gnome, etc… These are packages that need to be installed on top of your selected windows manager and an xorg.conf needed to correctly setup the video interface.
Note: If the cursor doesn’t show up right away, first hit: ctlr-alt-f1 then: ctrl-alt-f7 after which it ‘should’ show up…
Make sure to install, fbdev driver and xrandr utilities:
sudo apt update
sudo apt install read-edid xserver-xorg-video-fbdev x11-xserver-utils
#/etc/X11/xorg.conf
Section "Monitor"
Identifier "Builtin Default Monitor"
EndSection
Section "Device"
Identifier "Builtin Default fbdev Device 0"
Driver "fbdev"
EndSection
Section "Screen"
Identifier "Builtin Default fbdev Screen 0"
Device "Builtin Default fbdev Device 0"
Monitor "Builtin Default Monitor"
EndSection
Section "ServerLayout"
Identifier "Builtin Default Layout"
Screen "Builtin Default fbdev Screen 0"
EndSection
xrandr:
xrandr
xrandr --output HDMI-0 --mode 1024x768 --rate 60
xrandr (over serial/ssh)
xrandr -display :0.0 -q
xrandr -display :0.0 --output HDMI-0 --mode 1024x768 --rate 60
eMMC
Script to copy your microSD card to eMMC: (this will need these packages installed: initramfs-tools dosfstools rsync)
wget https://raw.githubusercontent.com/RobertCNelson/boot-scripts/master/tools/eMMC/bbb-eMMC-flasher-eewiki-ext4.sh
chmod +x bbb-eMMC-flasher-eewiki-ext4.sh
sudo /bin/bash ./bbb-eMMC-flasher-eewiki-ext4.sh
U-Boot Overlays
Full Documentation: [readme|https://elinux.org/Beagleboard:BeagleBoneBlack_Debian#U-Boot_Overlays]
Any issues:
#Any issues run:
sudo /opt/scripts/tools/version.sh
Enable:
#/boot/uEnv.txt
enable_uboot_overlays=1
To Disable: eMMC:
#/boot/uEnv.txt
disable_uboot_overlay_emmc=1
To Disable: HDMI VIDEO & AUDIO:
#/boot/uEnv.txt
disable_uboot_overlay_video=1
To Disable: HDMI AUDIO:
#/boot/uEnv.txt
disable_uboot_overlay_audio=1
To Disable: WL1835:
#/boot/uEnv.txt
disable_uboot_overlay_wireless=1
To Disable: BB-ADC:
#/boot/uEnv.txt
disable_uboot_overlay_adc=1
U-Boot: override detected capes
#/boot/uEnv.txt
uboot_overlay_addr0=<file0>.dtbo
uboot_overlay_addr1=<file1>.dtbo
uboot_overlay_addr2=<file2>.dtbo
uboot_overlay_addr3=<file3>.dtbo
U-Boot: disable auto-loading of detected capes
#/boot/uEnv.txt
disable_uboot_overlay_addr0=1
disable_uboot_overlay_addr1=1
disable_uboot_overlay_addr2=1
disable_uboot_overlay_addr3=1
U-Boot: load 4 more un-detected capes
#/boot/uEnv.txt
uboot_overlay_addr4=<file4>.dtbo
uboot_overlay_addr5=<file5>.dtbo
uboot_overlay_addr6=<file6>.dtbo
uboot_overlay_addr7=<file7>.dtbo
U-Boot: PRU Options (v4.19.x-ti)
#/boot/uEnv.txt
uboot_overlay_pru=AM335X-PRU-RPROC-4-19-TI-00A0.dtbo
U-Boot: PRU Options
#/boot/uEnv.txt
uboot_overlay_pru=AM335X-PRU-UIO-00A0.dtbo
U-Boot: Cape Universal
#/boot/uEnv.txt
enable_uboot_cape_universal=1
Comments
Any questions or comments please go to our TechForum: TechForum