This is a page about Renesas’s Cortex-A15 based R8A7791; R-Car_M2_Porter.
Availability
Boards:
- Y-RCAR-M2-PORTER-A at DigiKey
Basic Requirements
- Running a recent supported release of Debian, Fedora or Ubuntu on a x86 64bit based PC; without OS Virtualization Software.
- Many of the listed commands assume /bin/bash as the default shell.
- ARM Cross Compiler – Linaro: https://www.linaro.org
- Linaro Toolchain Binaries: https://www.linaro.org/downloads/
- Bootloader
- Das U-Boot – the Universal Boot Loader: http://www.denx.de/wiki/U-Boot
- Source: https://github.com/u-boot/u-boot/
- Linux Kernel
- Linus’s Mainline tree: https://git.kernel.org/pub/scm/linux/kernel/git/torvalds/linux.git
- ARM based rootfs
- Debian: https://www.debian.org
Baud Rate: 38400
ARM Cross Compiler: GCC
This is a pre-built (64bit) version of GCC that runs on generic linux, sorry (32bit) x86 users, it’s time to upgrade…
Download/Extract:
#user@localhost:~$
wget -c https://releases.linaro.org/components/toolchain/binaries/4.9-2017.01/arm-linux-gnueabihf/gcc-linaro-4.9.4-2017.01-x86_64_arm-linux-gnueabihf.tar.xz
tar xf gcc-linaro-4.9.4-2017.01-x86_64_arm-linux-gnueabihf.tar.xz
export CC=`pwd`/gcc-linaro-4.9.4-2017.01-x86_64_arm-linux-gnueabihf/bin/arm-linux-gnueabihf-
Test Cross Compiler:
#user@localhost:~$
${CC}gcc --version
#Test Output:
arm-linux-gnueabihf-gcc (Linaro GCC 4.9-2017.01) 4.9.4
Copyright (C) 2015 Free Software Foundation, Inc.
This is free software; see the source for copying conditions. There is NO
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
Bootloader: U-Boot
Das U-Boot – the Universal Boot Loader: http://www.denx.de/wiki/U-Boot
Depending on your Linux Distrubution, you will also need a host gcc and other tools, so with Debian/Ubuntu start with installing the build-essential meta package.
Download:
#user@localhost:~$
git clone -b v2013.01.01 https://github.com/u-boot/u-boot --depth=1
cd u-boot/
Patches:
#user@localhost:~/u-boot$
git pull --no-edit https://github.com/RobertCNelson/u-boot-boards v2013.01.01_porter
Configure and Build:
#user@localhost:~/u-boot$
make ARCH=arm CROSS_COMPILE=${CC} distclean
make ARCH=arm CROSS_COMPILE=${CC} porter_config
make ARCH=arm CROSS_COMPILE=${CC}
Programming: U-Boot
elinux Porter section on programming: https://elinux.org/R-Car/Boards/Porter#Updating_U-Boot
JP2: move to Jumper to 2-3
Start picocom
#user@localhost:~/u-boot$
sudo picocom -b 38400 --send-cmd "ascii-xfr -vvs" /dev/ttyUSB0
Switch on Board
Execute ls command
#PICOCOM
PORTER(M2W) SPI_LOADER(DDR3L) V0.20 2015.07.14
DEVICE S25FL032
PORTER(R-CarM2W) MiniMonitor SPI_BOOT
Work memory DRAM (H'40200000-)
DDR mode : DDR3-1600
2015.10.29 Ver0.10 ** Program on DRAM (H'40000000-) **
>ls
Load Program to Spiflash memory (U16:S25FL512S)
JP2(SPI_SEL) 1pin-Side! Setting OK? (Push Y key)
{code}
# JP2: move to Jumper to 1-2 and press "Y"
{code:title=PICOCOM}
---------------------------------------------------------
Please select,SPI-FLASH Save Area.
1:Loader Program : Program to execute on SecureRAM
SPI_Address = H' 000_0000-H' 003_FFFF
2:User Program : Program to execute on DRAM or SecureRAM
SPI_Address = H' 008_0000-H' 3FF_FFFF
---------------------------------------------------------
Select area(1-2)>
Press “2”
#PICOCOM
Select area(1-2)>2
-- User Program ----------------------------
Please Input User Program Start Address :
Use: “e6304000”
#PICOCOM
Please Input User Program Start Address : e6304000
Work RAM(H'50000000-H'53FFFFFF) Clear....
please send ! ('.' & CR stop load)
Type: CTRL-A, CTRL-S (file=u-boot.srec)
#PICOCOM
please send ! ('.' & CR stop load)
*** file: u-boot.srec
Press “y” to save u-boot into the SPI flash
#PICOCOM
$ ascii-xfr -vvs u-boot.srec
ASCII upload of "u-boot.srec"
699.0 Kbytes transferred at 3827 CPS... Done.
*** exit status: 0 ***
SPI Data Clear(H'FF) Check :H'00080000-000BFFFF,Clear OK?(y/n)
Flashing Complete
#PICOCOM
*** exit status: 0 ***
SPI Data Clear(H'FF) Check :H'00080000-000BFFFF Erasing..Erase Completed
SAVE SPI-FLASH....... complete!
-- Save (Program Start Address & Size ) -----
SPI Data Clear(H'FF):H'040000-07FFFF Erasing..Erase Completed
SAVE SPI-FLASH....... complete!
========== SPI Flash Sector1 Save Information =========
Program Start Address : H'E6304000
Program Size : H'0003A3E0
=========================================================
Hit Reset Button to verify u-boot was flashed correctly
#PICOCOM
>
PORTER(M2W) SPI_LOADER(DDR3L) V0.20 2015.07.14
DEVICE S25FL512
U-Boot 2013.01.01-00207-gefb7469873-dirty (Oct 24 2017 - 09:54:27)
CPU: Renesas Electronics R8A7791 rev 3.0
Board: Porter Board
DRAM: 1 GiB
MMC: sh-sdhi: 0, sh-sdhi: 1
SF: Detected S25FL512S with page size 256 KiB, total 64 MiB
In: serial
Out: serial
Err: serial
Net: Please set MAC address
sh_eth
Hit any key to stop autoboot: 0
=>
save defaults to spi flash
#PICOCOM
=> env default -a
## Resetting to default environment
=> saveenv
Saving Environment to SPI Flash...
SF: Detected S25FL512S with page size 256 KiB, total 64 MiB
Erasing SPI flash...Writing to SPI flash...done
Linux Kernel
This script will build the kernel, modules, device tree binaries and copy them to the deploy directory.
Download:
#user@localhost:~$
git clone https://github.com/RobertCNelson/armv7_devel ./kernelbuildscripts
cd kernelbuildscripts/
For v4.14.x-shmobile-armv7 (Longterm 4.14.x):
#user@localhost:~/kernelbuildscripts$
git checkout origin/v4.14.x-shmobile-armv7 -b tmp
Build:
#user@localhost:~/kernelbuildscripts$
./build_kernel.sh
Root File System
Debian 11
| User | Password |
|---|---|
| debian | temppwd |
| root | root |
Download:
#user@localhost:~$
wget -c https://rcn-ee.com/rootfs/eewiki/minfs/debian-11.3-minimal-armhf-2022-04-15.tar.xz
Verify:
#user@localhost:~$
sha256sum debian-11.3-minimal-armhf-2022-04-15.tar.xz
#sha256sum output:
575738843651de2962f251447f4742d4f33313d6f7f5edf282a401207f5e6646 debian-11.3-minimal-armhf-2022-04-15.tar.xz
Extract:
#user@localhost:~$
tar xf debian-11.3-minimal-armhf-2022-04-15.tar.xz
Setup microSD card
We need to access the External Drive to be utilized by the target device. Run lsblk to help figure out what linux device has been reserved for your External Drive.
#Example: for DISK=/dev/sdX
lsblk
NAME MAJ:MIN RM SIZE RO TYPE MOUNTPOINT
sda 8:0 0 465.8G 0 disk
├─sda1 8:1 0 512M 0 part /boot/efi
└─sda2 8:2 0 465.3G 0 part / <- Development Machine Root Partition
sdb 8:16 1 962M 0 disk <- microSD/USB Storage Device
└─sdb1 8:17 1 961M 0 part <- microSD/USB Storage Partition
#Thus you would use:
export DISK=/dev/sdb
#Example: for DISK=/dev/mmcblkX
lsblk
NAME MAJ:MIN RM SIZE RO TYPE MOUNTPOINT
sda 8:0 0 465.8G 0 disk
├─sda1 8:1 0 512M 0 part /boot/efi
└─sda2 8:2 0 465.3G 0 part / <- Development Machine Root Partition
mmcblk0 179:0 0 962M 0 disk <- microSD/USB Storage Device
└─mmcblk0p1 179:1 0 961M 0 part <- microSD/USB Storage Partition
#Thus you would use:
export DISK=/dev/mmcblk0
Erase partition table/labels on microSD card:
sudo dd if=/dev/zero of=${DISK} bs=1M count=10
Create Partition Layout:
With util-linux v2.26, sfdisk was rewritten and is now based on libfdisk.
#Check the version of sfdisk installed on your pc is atleast 2.26.x or newer.
sudo sfdisk --version
#Example Output
sfdisk from util-linux 2.27.1
#sfdisk >= 2.26.x
sudo sfdisk ${DISK} <<-__EOF__
1M,,L,*
__EOF__
Format Partition:
With mkfs.ext4 1.43, we need to make sure metadata_csum and 64bit ext4 features are disabled.
As the version of U-Boot needed for this target CAN NOT correctly handle reading files with these newer ext4 options.
#mkfs.ext4 -V
sudo mkfs.ext4 -V
mke2fs 1.43-WIP (15-Mar-2016)
Using EXT2FS Library version 1.43-WIP
#mkfs.ext4 >= 1.43
for: DISK=/dev/mmcblkX
sudo mkfs.ext4 -L rootfs -O ^metadata_csum,^64bit ${DISK}p1
for: DISK=/dev/sdX
sudo mkfs.ext4 -L rootfs -O ^metadata_csum,^64bit ${DISK}1
Mount Partition:
On most systems these partitions may be auto-mounted…
sudo mkdir -p /media/rootfs/
for: DISK=/dev/mmcblkX
sudo mount ${DISK}p1 /media/rootfs/
for: DISK=/dev/sdX
sudo mount ${DISK}1 /media/rootfs/
Install Kernel and Root File System
To help new users, since the kernel version can change on a daily basis. The kernel building scripts listed on this page will now give you a hint of what kernel version was built.
-----------------------------
Script Complete
eewiki.net: [user@localhost:~$ export kernel_version=5.X.Y-Z]
-----------------------------
Copy and paste that “export kernel_version=5.X.Y-Z” exactly as shown in your own build/desktop environment and hit enter to create an environment variable to be used later.
export kernel_version=5.X.Y-Z
Copy Root File System
#Debian; Root File System: user@localhost:~$
sudo tar xfvp ./debian-*-*-armhf-*/armhf-rootfs-*.tar -C /media/rootfs/
sync
Set uname_r in /boot/uEnv.txt
#user@localhost:~$
sudo sh -c "echo 'uname_r=${kernel_version}' >> /media/rootfs/boot/uEnv.txt"
Copy Kernel Image
Kernel Image:
#user@localhost:~$
cat ./kernelbuildscripts/deploy/${kernel_version}.zImage ./kernelbuildscripts/arch/arm/boot/dts/r8a7791-porter.dtb > ./kernelbuildscripts/deploy/${kernel_version}.zImage.dtb
sudo cp -v ./kernelbuildscripts/deploy/${kernel_version}.zImage.dtb /media/rootfs/boot/vmlinuz-${kernel_version}
Copy Kernel Modules
#user@localhost:~$
sudo tar xfv ./kernelbuildscripts/deploy/${kernel_version}-modules.tar.gz -C /media/rootfs/
File Systems Table (/etc/fstab)
#user@localhost:~/$
sudo sh -c "echo '/dev/mmcblk0p1 / auto errors=remount-ro 0 1' >> /media/rootfs/etc/fstab"
Remove microSD/SD card
sync
sudo umount /media/rootfs
Comments
Any questions or comments please go to our TechForum: TechForum