Device setup including APN configuration for VIoT-Flex IoT SIM Cards
Quickly connect VIoT-Flex SIMs to most cellular modules with our concise, user-friendly instructions.
Setup procedures can vary across different device modules. Always refer to the specific device manual for accurate guidance.
Step 1: Make Sure your Velocity IoT SIM is active
- For enterprise accounts check that your SIMs have been added to your account. If assistance is needed contact support@velocityiot.io
- Standard platform users should ensure their SIMs are added to velocityiot.net their account. If this step is incomplete, refer to the guidelines for account creation and adding SIMs.
Step 2: Insert the SIM in your device
- Power off the IoT device before inserting the SIM card.
- Locate the SIM card slot, which is typically on the side or back of the device.
- Carefully insert the SIM card in the correct orientation as shown in the device’s instructions or by the design of the slot.
- Once the SIM card is securely in place, the device is ready for network connection.
Step 3: Device Configuration
Set device APN
- Power off your device and insert the SIM card.
- Once powered on, set the device to utilize the APN: “flolive.net”
Configuring the APN with the following AT command should work on most modules
AT+CGDCONT=1,“IP”,“flolive.net”
After APN configuration, you should be able to fetch an IP address and initiate a PPP connection. Always consult your device’s manual since settings differ and activation of the session may be required.
Setting the Device as Data Centric
Optimally, set your module to attach as a data-centric device. Refer to the manufacturer’s documentation for specific instructions.
Enable Device Roaming
Roaming must be enabled for all devices on the VIoT-Flex SIMs. Refer to the manufacturer’s documentation for specific instructions.