DFROBOT PN: FIT0723

Good morning, I am looking for a crossover item of the MFG part number FIT0723 DFROBOT. Can you help me find this information?

Thank you

Hello claudiar.vmindustria, welcome to the TechForum! It looks like this specific design (dimensions and features) is the only one of its kind. There are some slightly larger boxes that have a similar design you can look at. Here is a list of options I could find that have similar surface area measurements, click HERE.

I would say that the most similar are the following, both with clear covers and mounting flanges. The only difference between the two is the water ingress IP ratings, with the PN-1324-ACMB having the higher IP68 rating:

  • PN-1324-CMB Box Plastic 6.73"L X 4.76"W, Polycarbonate, Clear Cover, IP65 rated
  • PN-1324-ACMB Box Plastic 6.73"L X 4.76"W, Polycarbonate, Clear Cover, IP68 rated

Here’s a link to a side-by-side comparison.