ED-HMI3020-101C how to connect m.2 ssd

Question About M.2 Storage Support on ED-HMI3020-101C

Hi,

I recently purchased an ED-HMI3020-101C, and according to the specifications, it supports M.2 storage. However, I am unable to find a connector for an M.2 SSD.

Do I need a different type of display to use M.2 storage?

Best regards,
Endre

Greetings,

It appears that the SSD is meant to be ordered as a factory-configured option. It’s quite possible that devices ordered without would omit population of the connector as a cost-saving measure.

Hi,

OK, then I’ll have to order a different type. Thanks, that was a great explanation!

Best regards
Endre

Hello @endre and @rick_1976,

This is EDATEC Technical Support.

Rick is absolutely correct. For the ED-HMI3020-101C series, the M.2 SSD is a factory-configured option. If the device was ordered with the “Without SSD” configuration (Code ‘0’), the necessary M.2 connector and related circuitry are not populated on the board.

To ensure you get the M.2 storage in your next order, please refer to our Ordering Code guide. You will need to select a model where the SSD digit is specified as ‘1’ (128GB) or ‘2’ (256GB).

Important Note for Pi 5 Models: As shown in the datasheet note: Since the Raspberry Pi 5 does not have onboard eMMC, when selecting a model, you must choose at least one storage medium: either an SD card or an SSD, to ensure the system is bootable.

You can view the full specifications and ordering details here: https://edatec.cn/docs/hmi3020-101c/ds/

Best regards, EDATEC Technical Support Team