TDK EPCOS offers a wide variety of useful magnetic and passive components. Today isn’t about those components, though. Today is about the closest you’ll likely ever come to holding a lightsaber in your hand - their B54324D5120A140 PiezoBrush cold plasma tool. This is a piezoelectric direct discharge (PDD) tool that generates a cold active plasma (temperatures of less than 50C), which is used to increase surface energy of various materials highly efficiently as well as used for sterilization and germ/odor control. What does this fascinating device come with?
Per the product’s datasheet, the PZ3 comes supplied with everything you need to make the device function. Lightsaber wooshing noises while in use will have to be supplied by the end user, but aren’t strictly required for proper functionality.
You can also source one of the ‘wear part’ consumable module replacements from DigiKey: their standard module is B54321P5100A020. Unfortunately, the nearfield module B54321P5100A120 isn’t available through us for direct order at this time.