Not sure if this is the correct category. I am a land surveyor, and I have a robotic total station that is used to measure the location of a prism. It is robotic in the sense that it is controlled remotely by a “remote controller”. In order for the total station to “find” the prism, the remote controller emits a laser beam at 785 nm. It is a Class I laser device. There is a receiving window on the total station and inside a beam detector which receives the laser beam emitted by the remote controller. This system is not working on my instrument, and I’d like to troubleshoot and find a way to determine whether the laser beam is being emitted in the first place. What device or electronic component (other than my eyes, not safe) can be used to determine whether the laser is being emitted? A photodiode? A photodetector? Something else? Any tips on how to set up a circuit for this purpose would be most appreciated.
I’m not sure it helps, but this video shows what I am dealing with and might give context.
https://youtu.be/sHYFE9gzHEM