Is there a relay that can be used in a dusty environment?

Question:

Is there a relay that can be used in a dusty environment?

Block

Answer:

Consider a plastic-sealed relay for use in a dusty atmosphere.

Block

Explanation:

If a relay is used in an atmosphere in which dust is generated, dust may enter the relay and become trapped between the contacts, preventing the relay from closing. Also, if conductive objects such as wire chips enter the relay, contact failure or short circuit may occur.
In such a case, take measures against dust or use a plastic-sealed relay.

For more information, see Safety Precautions for All Relays:1. Selecting Relays.

Block

Quick tips

Even when using a plastic-sealed model, accumulation of dust on a printed circuit board may degrade the insulation of the circuit. It is recommended to take measures to seal the control board.

Block

Please visit the link below to see this product line on the Digi-Key website
Relays | Digi-Key Electronics


This FAQ has been brought to you courtesy of




Please click the link below to view the original FAQ
https://components.omron.com/us-en/faq/relays/FAQE10009