Lithium Content in ER2450-T

Background:
When shipping lithium batteries in a product with some carriers, the lithium content per cell and per package determines the labeling requirements and shipping restrictions.

Question:
Is is reasonable to assume the lithium content of an ER2450-T is similar to a TL-2450-P?

They are the same form factor and similar capacity. The datasheet for the TL-2450 lists the lithium content as approximately 0.2g. The ER2450-T datasheet does not include any information on approximate lithium content. I’ve contacted Jauch Quartz (manufacturer of the ER2450-T), but I don’t expect to get very far with that avenue due to the low volumes involved.

Hello TRMT,
Thank you for posting on the Digikey TechForum.
The only information I was able to find were from the material safety datasheets.
TL-2450/P
MSDS

ER2450-T
MSDS

They showed similar weight percentage in lithium content.

Great finds! Thank you very much! Thank you also for the quick response.

Just a quick update for anyone in the same boat. Jauch Quartz did eventually respond to my inquiry. Their official value is 0.143g.