Logic or Embedded/I Would Like to Gain in Amperage by So Much

So,

Here it is: what mathematic approach would I need so that my mA is gained by 5mA?

I am asking because I have a GPIO peripheral handling so much mA and I need to have a gain in mA to handle a driver (DM542T).

So, I was guessing on the math handling around the approach to get from 4mA to about 8mA or 9mA of current. I will be testing of course…

Here is the issue: is using older technology that wholesomely is broken but parts may be salvaged still legal?

I mean, would I need to purchase new parts? And, if I need to purchase new parts, what exact current gain should I be searching to attain?

For instance: https://www.digikey.com/short/58twnm0p which would bring someone to a Diodes Incorporated BSS138DW-FDICT-ND.

I see in the datasheet some specifications for, say, this exact match which is probably what I do not need right now but just to say:

| BVDSS | RDS(ON) Max      | ID Max TA = +25°C |
|  50v  | 3.5Ω @ VGS = 10V |       200mA       |

How can I really interpret these STEM meanings and the approach I would need to take to get my dial turning correctly?

I am not finding a way to understand everything when I need to be able to understand a bit.

So and for now, the BeagleY-AI from beagleboard.org will be used as a test case on my learning path. Right now, I have a cool motor, a driver, and the BeagleY-AI driving the GPIO peripheral to handle some fan-tan-tastic GPIO driven linear actuator moves.

I am not sure if you caught it or not but I have a cool motor. ha.

All jokes aside, the motor is way too cool for me to believe it was once so darn hot that I could not touch it. I got lucky as usual.

Resistors, Transistors, and LEDs will be in the mix but, and I again state this idea, I need the math behind how to understand what it is I am looking at now (this datasheet). Okay. Done for now.

Hello,
Welcome to the forum. I’ll do some checking on this and post the information I find.

It appears that the essential question here involves providing a modest boost to a few microcontroller I/O pins.

The datasheet for the drive mentioned gives a representation of the inputs on page 6. Figure 2 offers an illustration of how the job could be done using some extra transistors of the sort mentioned.

Thank you.

So, are you marking this solved because of the fact that I only need to configure a few mA “boost” from some I/O? If so, fine by me.

I guess I am just not fully understanding how to gain in mA per use of the I/O (GPIO) while the I/O is being used.

But…if this stands. Okay.