Hey All,
I had submitted a ticket regarding the product information for P/N: MAX16903SAUE50/V+T. The voltage input max shows 28 VDC while the data sheet indicates it’s 42 VDC. The reply from the ticket was the info was correct as is. Am I missing something?
@manchester49123
The 42vdc is the absolute max it can handle. The document shows that would be for less than 1 second though.
The nominal maximum that it can handle without damage would be 28vdc.
I agree with Nathan_2268.

Appreciate you guys clearing up my confusion. Also appreciate the quick response!