------Question for SC1512-A4 Please Put your question below------
When I look for the RP2354B, I noticed it is listed only under a 7” or 13” reel consisting of 500 or 2500 parts respectively. If I only need 10 individual ICs, is there a way to order that?
There seems to be an option to order individual ICs of the RP2350.
Hi neil.blatzheim,
Welcome to the TechForum.
The SC1512(13)-A4 and the SC1512-A4 are both the exact same RP2354B loaded into 2500 piece or 500 piece reels. We order both the 7" and 13" sizes but we sell either one in quantities down to one piece, so you can place an order for 10 pieces of either part number and you’ll be getting the same part.
1 Like