I want a part that has one input wire and two possible ouputs. This part will be constantly receiving a zero, and will start outputting zero. When I send this part a 1 I want the output to switch to a 1 and stay there even though the part is receiving zeros. So now that the part is outputting 1 and is receiving zero, once I send another 1 I want the output to switch to a zero. I essentially only want the output to switch what it is when this part receives a one, and then I want it to hold that output.
What voltage and current levels do you want?
What’s your target price?
Hello,
Thank you for contacting the Technical Forum.
That is one of the ways to use a Flip Flop. You turn it into a “Toggle”, or “T”, flip-flop by tying J and K to logic “1”, tying “S” and “R” to logic “0”, and using the clock pin as the input. (Note, some flip-flops have inverted logic on some of these pins, like 1), so you would tie it low rather than high for this application).
Every time the clock sees a positive-going edge (zero to one transition) the output changes to opposite of previous state.