RE: LCD Cape for the BBB/BBG

Hello,

I am using a BBG to display an OS on my Debian Distro. I received help once or twice before on another service but I thought I would come here to see if anyone knew of my issue.

…

Here is the cape:
http://wiki.seeedstudio.com/Seeed-Studio-BeagleBone-Green-LCD-Cape-with-Resistive-Touch/

…

Here is my version.sh file. Sorry for the long winded approach.

debian@forths:~$ sudo ./version.sh
git:/opt/scripts/:[e457c010efc76c4e6fecccb7a5f7ff9b0597c4c0]
eeprom:[A335BNLTBBG1BBG116044099]
model:[TI_AM335x_BeagleBone_Green]
dogtag:[BeagleBoard.org Debian Image 2018-10-07]
bootloader:[microSD-(push-button)]:[/dev/mmcblk0]:[U-Boot 2019.04-00002-gf6fce6c5bf]:[location: dd MBR]
bootloader:[eMMC-(default)]:[/dev/mmcblk1]:[U-Boot 2019.04-00002-gf6fce6c5bf]:[location: dd MBR]
UBOOT: Booted Device-Tree:[am335x-boneblack-uboot-univ.dts]
UBOOT: Loaded Overlay:[AM335X-PRU-RPROC-4-14-TI-00A0]
UBOOT: Loaded Overlay:[BB-BONE-eMMC1-01-00A0]
UBOOT: Loaded Overlay:[BB-BONE-LCD5-01-00A1]
UBOOT: Loaded Overlay:[M-BB-BBG-00A0]
kernel:[4.19.94-ti-r35]
nodejs:[v6.17.0]
/boot/uEnv.txt Settings:
uboot_overlay_options:[enable_uboot_overlays=1]
uboot_overlay_options:[uboot_overlay_pru=/lib/firmware/AM335X-PRU-RPROC-4-14-TI-00A0.dtbo]
uboot_overlay_options:[enable_uboot_cape_universal=1]
pkg check: to individually upgrade run: [sudo apt install --only-upgrade ]
pkg:[bb-cape-overlays]:[4.4.20190922.0-0rcnee0~stretch+20190922]
pkg:[bb-wl18xx-firmware]:[1.20190227.1-0rcnee0~stretch+20190227]
pkg:[kmod]:[23-2rcnee1~stretch+20171005]
pkg:[librobotcontrol]:[1.0.4-git20190227.1-0rcnee0~stretch+20190327]
pkg:[firmware-ti-connectivity]:[20180825+dfsg-1rcnee1~stretch+20181217]
groups:[debian : debian adm kmem dialout cdrom floppy sudo audio dip video plugdev users systemd-journal i2c bluetooth netdev cloud9ide gpio pwm eqep admin spi tisdk weston-launch xenomai]
cmdline:[console=ttyO0,115200n8 bone_capemgr.uboot_capemgr_enabled=1 root=/dev/mmcblk0p1 ro rootfstype=ext4 rootwait uboot_detected_capes=BB-BONE-LCD5-01, coherent_pool=1M net.ifnames=0 quiet]
dmesg | grep remote
[ 1.443939] remoteproc remoteproc0: wkup_m3 is available
[ 1.445968] remoteproc remoteproc1: 4a338000.pru is available
[ 1.446562] remoteproc remoteproc2: 4a334000.pru is available
[ 1.597498] remoteproc remoteproc0: powering up wkup_m3
[ 1.597626] remoteproc remoteproc0: Booting fw image am335x-pm-firmware.elf, size 217168
[ 1.601247] remoteproc remoteproc0: remote processor wkup_m3 is now up
dmesg | grep pru
[ 1.445968] remoteproc remoteproc1: 4a338000.pru is available
[ 1.446106] pru-rproc 4a338000.pru: PRU rproc node pru@38000 probed successfully
[ 1.446562] remoteproc remoteproc2: 4a334000.pru is available
[ 1.446654] pru-rproc 4a334000.pru: PRU rproc node pru@34000 probed successfully
dmesg | grep pinctrl-single
[ 1.024409] pinctrl-single 44e10800.pinmux: 142 pins, size 568
dmesg | grep gpio-of-helper
[ 1.038236] gpio-of-helper ocp:cape-universal: ready
lsusb
Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
END

…

Seth

P.S. If anyone can figure out what is incorrect, please let me know. I am on 4.19.94-ti-r35 and Debian Image 2018-10-07.

Hello Again,

Please forget what I was saying.

Seth

P.S. If that version.sh script helps anyone, good. Outside of that idea, hack!

@silver2row, little confused, does it work?

If it doesn’t, do you have usb power plugged into both the beaglebone green and the seeed lcd?

Regards,

Hello @RobertCNelson,

It works.

Seth

P.S. I am sorry to issue this statement after I started to mess w/ it more. I figured out my concern. It worked all along. I just did not remember exactly what happened last time I tried to make it work.