------Question for AIPXE-325X4A Please Put your question below------
Hi, need to know the box quantity of AIPXE-325X4A and 0297002. For a try out I need to order 50 pcs of each item.
------Question for AIPXE-325X4A Please Put your question below------
Hi, need to know the box quantity of AIPXE-325X4A and 0297002. For a try out I need to order 50 pcs of each item.
Hi,
Thank you for your inquiry. Connector enclosure AIPXE-325X4A is sold in a quantity of 1= 1
so, if you require 50 connector enclosures you will need to order a quantity of 50.
For 0297002 I am unable to verify that part number in our system. You will need to provide the DigiKey part number.
Hi Justin,
Thank you for your feedback.
Regarding the datasheet, 0297002.H will be packed by 100 pcs, correct?
That partnumber is ordered ( see attachement ).
Please verify if it will be about a 100 pcs package.
INVOICE_123507279.pdf (110 KB)
Hi,
2A fuse 0297002.H-ND is also sold in quantites of 1 =1 fuse. If you require a full manufacturer pack quantity of 100 you will need to order a quantity of 100
Dear Justen,
That is not very clear with the eye on the datasheet to be honest.
Unfortunately, we now have double shipping costs and custom clearance.
Can you assist and send 50 pcs of that fuse with our reference: REDACTED?
That will be very helpfull.
The TechForum is for technical questions, for order support you will need to contact customer.service@digikey.com.
Regarding part 0297002.H-ND, the manufacture quantity is 100 per box. But at DigiKey we buy that box and then we will break open that box so a customer can order just 1 piece from it, instead of a full 100 piece box.
Notice the box icon next to 100 in the price break. This denote that this is the manufacturer’s standard packaging for 0297002.H, as shown below the price breaks.
Hello arjan.jansen,
If you have a PO to send in for an order, you can send it to orders@digikey.com.
We only handle the Technical questions, and have nothing to do with the ordering process.
Hi arjan.jansen,
To elaborate on what @Steven_14444 is describing, here at DigiKey, we receive full boxes of parts from all of our vendors and then we can either sell those full boxes or open them up and sell any quantity our customers need, typically all the way down to one piece.
As such, with only a very few exceptions, when you order a unit quantity of “1” of any part we sell, you will receive one single piece of that part number.
So regardless of whether you order a unit of “1” of the 0297002.L, 0297002.H, 0297002.U, or 0297002.WXNV, you will get 1 piece, not a full manufacturer’s box quantity of that part. If you order a quantity of “50”, you will be shipped 50 pieces.