Sometimes it takes a little more effort to figure out what a part may look like than others. We try to obtain accurate pictures, but can’t always guarantee it will look exactly like the one we display. It’s especially frustrating when manufacturers only provide series photos or generic photos of their products on part pages or even datasheets. This is one of the reasons why 2D drawings can be so beneficial.
Where is the drawing for 95-EBAU14-10-ND?
When you search for this part on our site, there is no image to represent this part at the moment. When you check the datasheet, there also is no representative image. Eaton’s site does get a little warmer, but the picture on their page is also only a photo of a part in the same series.
Eaton Site Picture
Datasheet Drawing Link
The datasheet does have documentation included for the most accurate depiction. The second page, under the section that says Drawings, there is a link that says EBAU14-10 Technical Drawing. This is the most accurate “picture” for how the part looks at the moment.
Other Details About the Part
If you want to know some interesting things about this part according to the drawing, the part is compatible with 3-Phase VAC. It also has 3 circuit breakers installed for each pole. I believe they are indicated on the top drawing above the main part shown as A B and C. The input cord is a NEMA L21-30 Plug. It has 6 NEMA plugs, 12 IEC C13 plugs, and 3 more IEC C19 connections. The outlets are all plug types so that people cannot easily touch the metal contacts when energized.