What is the contact resistance of a basic switch?

Question:

What is the contact resistance of a basic switch?

Block

Answer:

The contact resistance is the resistance value (the initial resistance value is the CR before shipment) between the energized terminals when the contacts are in contact with each other. The resistance value of the contact area includes the conductor resistance of the spring and terminals.
The NC side (b-contact) is measured in the FP state and the NO side (a-contact) is measured in the TTP state.

Block

Explanation:

The contact resistance is the resistance value (the initial resistance value is the CR before shipment) between the energized terminals when the contacts are in contact with each other. The resistance value of the contact area includes the conductor resistance of the spring and terminals. The NC side (b-contact) is measured in the FP state and the NO side (a-contact) is measured in the TTP state.

Keep the following in mind to increase contact pressure:

  1. The larger the OF, the larger the contact pressure.
  2. The larger the OF, the larger the contact pressure.
  3. The contact pressure is higher at the FP and TTP points during the stroke. Please note that in particular, contact pressure becomes almost zero near the point of contact switching (OP point, RP point), causing contact instability and potential chattering.

Block

Product category

Switches Basic Switches


Classification

Selection, Characteristics


Related keywords

Basic Switch
Contact Resistance
Unstable Contact
Oxidation
Sulfurization
Contact Pressure
F-S Characteristics
CF-S Characteristics

Block

Please visit the link below to see this product category on the Digi-Key website
Switches | DigiKey Electronics


This FAQ has been brought to you courtesy of




Please click the link below to view the original FAQ

https://components.omron.com/us-en/faq/switches/FAQE20018