What is the difference between a Siemens type C and type FC PLC?

This article is part of a guided learning series on building our understanding of the Siemens S7-1200 PLC.

:pushpin: Canonical Article: Navigating Siemens S7-1200 PLC model numbers
:blue_book: Learning Companion (Q&A): Learning Companion Navigating Siemens S7-1200 PLC model numbers

You are reading: Question 3

What is the difference between type C and type FC PLC?

Definition of failsafe

The failsafe industrial automation equipment is designed to protect the user. There are several universal properties:

  • Elevated testing with high mean time between failure.

  • Tiered rating using scales such as a SIL (Safety Integrity Level) and Performance Level (PL) to indicate the level of danger associated with the machine. For instance, a machine capable of causing death will be guarded and rated higher than a machine limited to bruising. The featured PLC is rated for:

    • SIL 3 according to IEC 61508

    • Performance level PLe according to ISO 13849-1

  • Redundancy as described in this article exploring an e-stop connected to a dedicated safety relay

  • Protected against short-circuit to supply or return. A pulsed signal is often incorporated.

  • Independance from conventional control logic. In the case of a combinational PLC featured in the canonical article, we can assume the PLC included redundant circuit to continue protection even when the main processor experiences a fault or other logic error.

  • Simplified programming to reduce the risk of error.

Industrial automation safety equipment is typically yellow or red in color.

Answer

The type C (e.g., CPU1215C) is the standard PLC. The type FC (e.g., (CPU 1215FC) contains the core functionality of the type C but adds a layer of fail-safe technology.

Tech Tip: Originally the C stood for “compact”. We could therefor describe the FC as a compact PLC with an integrated fail-safe option. The fail-safe hardware is identified by the yellow color. A subtle example is shown in Figure 1 where the left and right centers of the PLC contain a yellow band.

:writing_hand: Article by Aaron Dahlen, LCDR USCG (Ret.), Application Engineer at DigiKey