------Question for FSP2000-20FM Please Put your question below------
I am looking for a 2000W output server power supply that does not drop the output to 1000W when connected to a 100VAC input. Came across this PSU module but cannot confirm if FSP2000-20FM can output 2000W at 100VAC input as well? Datasheet is a bit unclear.
Thanks
Greetings,
Unfortunately, what you’re looking for might be in the same product class as blinker fluid and board stretchers.
Getting 2 kW from a 100V source means an 80+ supply has to draw roughly 25A. IEC320-C13/14 connectors are only rated to 15A and the familiar NEMA 5 connectors only go to 20, so any supply using those can’t do the job in an installation built to spec.