230V EURO to US adapter

Hello,

I am looking for assistance finding an adapter to convert a 230V EURO plug to fit an US 230V outlet. The receptacle in the outlet has horizontal openings instead of vertical.

Add images

Hello @dsmeglin and welcome to the forum! Unfortunately I don’t believe we stock an adapter that converts between these two connector types. You’ll have to seek this out through a retailer, though if it helps I do have some information that might help:
The proper name for that outlet receptacle is a NEMA 6-15R, so searching for that will net you better results. If you just search for a “US adapter” you’ll end up with tons of results that are just for the regular 120V plugs, but if you search for “NEMA 6-15” you’ll get this results relevant to this specific type of outlet.

What is the other end of the power cord that you have? If connector is IEC 320 C13, you can use one of these cables instead.

I was able to use 1939-1022-ND. Thank you for your assistance