4604X-101-512LF

Is the Bourns resistor array obsolete? I am trying to find the following part:4604X-101-512LF.

Nothing comes up in the search option. Can someone confirm if it is still in use?

@bartlomiej.odjas

I am not seeing that we list the “512” (5.1KΩ) value for that series.
We list the 4604X-101-513LF (51kΩ) for that series.
4604X-101-513LF Bourns Inc. | Resistor Networks, Arrays | DigiKey

For an item that is 5.1KΩ I found the CSC04A015K10GPA-ND.
CSC04A015K10GPA Vishay Dale | Resistor Networks, Arrays | DigiKey

It may be that the 4604X-101-512LF was obsoleted. It is also possible that the “4604X-101-512LF” was not a common enough item to have stocked.

Hi bartlomiej.odjas,

If you are just looking for a small quantity rather than the 2000 pcs MOQ required order for the non-stocking CSC04A015K10GPA, and you have a little extra space on your board, perhaps the following part is worth considering:

It is just the 5-pin version of the same series as the part you are looking for. To make it work, it would need to fit in the space you have available and you would just clip off the 5th pin. To fit, you would need an extra 2.54mm of clearance past your part on the pin4 side.

As of this writing we have over 1000pcs in stock, though once depleted, it will become a non-stocking part for us.

Hi David,

Unfortunately it won’t work as the required part is for the existing design.

It must be a 4 pin SIP and 5k1.

As I tried to explain, if you have physical room, then the 4605X-101-512LF could work for you if you clip pin 5. Essentially, that turns it into the exact part you need other than that it will extend 0.1" further past pin 4.

Oh I see. Sorry David, I missed your point.

Unfortunately I cannot use this part. This is more down to the nature of industry (aerospace). If it is not a form, fit, function part, then a full requalification would be needed. It would not be accepted on this ground. Many thanks for your input anyway.

Ahh, that’s too bad.

The CSC04A015K10GPA that @Nathan_2268 mentions above would be a form-fit-function match. Note, however, that it is NOT ROHS compliant (it has tin-lead (Pb) coated pins). Of course, that may not be an issue for some aerospace applications which require maximum reliability of solder joints.

The primary drawback to the CSC04A015K10GPA is that we do not normally stock it, so it would require a significant lead-time for delivery and an MOQ of 2k pieces.