5131-CIL12302G001-ND 4G Backhaul confirmation question

Hi there,

I have a confirmation question regarding the 5131-CIL12302G001-ND please.

The detailed description for the product is: “4G 802.11 b/g/n, LoRaWAN Gateway Ethernet, RJ45”

Can you please confirm if this is indeed the 4G version as stated in the detailed description, as Elecrow sells a version with only WIFI and ethernet backhaul only as well as a version that includes 4G cellular internet as well. (The global 4G version is an option in the dropdown menu for an additional 6$)

Unfortunately the SKU is CIL12302G for all variants (868MHz, 915MHz with and without 4G) so I cannot discern is the product sold on DigiKey is indeed the 4G variant from elecrow.

Thank you,

Kind regards,

Hermann Havenstein

I am checking on this one. Will let you know when I have the information.

The version DigiKey sells is not a 4G global version because 4G version is a new one launched just recent months from Elecrow and the version that we sell is the regular one with 868 mhz below.

ThinkNode G1 Indoor 8 Channels LoRaWAN Gateway Powered By SX1302 Chip-868MHz

Hi Karl,

Thank you very much for confirming so quickly :slight_smile:

I hope DigiKey will make the decision to stock the 4G version in the future.

Kind regards,

Hermann Havenstein

Hello, I see there are two versions CIL12302G001 and CIL12302G002. Which version includes 4G?

The two part numbers are the same with the exception of the frequency.

Part number CIL12302G001 is 915MHz.
Part number CIL12302G002 is 868MHz