Yeah I did find find that link and ended in the same spot. I messaged Deltrol so I’m hoping to find a vendor on that if they come through. Ive found less on the Hsinda relay.
Hello everyone!
Need help with driver choosing:
We are looking for a remote driver with requirements below:
110-277 VAC input
24VDC output
240W power minimum
0-10V dimming
Class 2
IP 20 (minimum rating)
Also we need to know the maximum wire length for the driver you can propose.
Earlier we have chosen this one HLG-240H-24B MEAN WELL USA Inc. | Power Supplies - External/Internal (Off-Board) | DigiKey
but it’s class 1 (maybe you can advise a special box for it)
Thank you!
Hello engineer_GBC
I was not able to locate a led driver like part number HLG-240H-24B which is class 2.
If you would like a box for part number HLG-240H-24B, please provide specifications for the box you would need. Click here for a link to the boxes we offer.
Hello, @Becky_1523 , @Steven_14444
Thank you for quick response!
Can I use this one as a fire safe box to improve the driver to class 2?
Also we need to know the maximum wire length for the driver
HLG-240H-24B MEAN WELL USA Inc. | Power Supplies - External/Internal (Off-Board) | DigiKey.
The chandelier lenght is about 23’ from top to the last light sourse.
How far can we mount the driver from the fixture?
Thank you!
Hello,
I am checking on this. Will let you know when I have an answer.
Here is the mfg. reply to this,
A 23-foot distance isn’t too far; just make sure they use the right output cable to prevent voltage drop.
I am looking for an Infineon IGBT stencil pattern to apply thermal paste to their 62mm modules. Per their application note, AN2012-05, Infineon states to reach out to the distributors for these stencils in section 8.2.2:
" The module-specific drawings of a printing stencil can be obtained from the distribution partner for Infineon modules. "
Please advise, and thanks for your help!
I have submitted an inquiry for this. We will update you when we hear back.
Any update here? Thanks!
hello, I’m trying to find an HDMI port for the sony playstation 5. do you know if this is something you guys have?
Hello technicdub, Welcome to the DigiKey TechForum.
Looking at the specs for the PS5, it looks like they use a 2.1 HDMI protocol. HERE is list of the 2.1 HDMI ports that we currently carry.
The Product Specialist is requesting the specific model number of the Infineon IGBT. Can you please provide this?
Current part number: FF450R12KE4
I am open to alternatives should the manufacturer have better support.
Thank you for this information arete.audio. I have passed this on to our product specialist and we will update you once we have received a response.
I am looking for a cross for my EBM A2D200-AA04-48 fan.
Specs:
265/460v
60hz
0,11A
65W
3100rpm
p/n 613450-IG
7 wires
Hello, it looks like we received a request for this one already. We will get you an answer as soon as we have the information.
Sounds great! Will I receive a response via email or on here?
Checking in, any update from the manufacturer?
Please see attachment for what the manufacture sent to us.
Silk Screen for 62mm modules 75µm (2016-05-19) Model.pdf (92.3 KB)