Ask questions and get support on any DigiKey Product that doesn’t fit into one of our technology categories.
To post, simply log in using your “My DigiKey” account credentials or sign-up for your own log-in here.
Ask questions and get support on any DigiKey Product that doesn’t fit into one of our technology categories.
To post, simply log in using your “My DigiKey” account credentials or sign-up for your own log-in here.
Hi there,
Is there a 5 pin version of the Adafruit magnetic connector Nr. 5467?
If so, what’s the part number?
Hello,
Take a look at part number 5413. I believe this is the one you are looking for.
Hi Karl,
It is a 5 pin connector but not the same model as the 5467 whose housing serves my purposes better.
But I will use the 5413 if there isn’t a 5 pin connector of the 5467 make.
Hi, I am looking for a push button switch that is always completing one circuit, unless it is held depressed, then it opens that circuit and completes another. It should return Could you please point me in the right direction?
Hello dawsonmarch.stu
You should be looking for an on-mom type of switch. Click here for options.
I have an (actually 2) EZVIZ BC1 camera that has become foggy inside. EZVIZ offers no support but buying a new camera. I have taken the camera apart and identified the lens part. It is marked F-243 and 2880 and a QR code I cannot read. It also has a very small label with some kind of QR code and the numbers 14388583 and 201902565. Would you have this component?
Hi pegarvidsson,
Welcome to the DigiKey tech forum community.
I wasn’t able to find that exact lens. I found nothing within our stock with that part number of the lens F-243 nor 2880. When I searched for more info on the camera itslef. it seems to be the lens is the 28mm diameter but I found nothing in our inventory at that size lens, I’m not sure how accurate that information was since I did not find an actual spec sheet or data sheet on it.
Sorry for the inconvenience.
Here is the category of optical lenses I looked through.
I’m currently in a situation where I require a continuous rotation servo to spin a dowel attached to a small foam prop at speeds of ~1000RPM (For a film’s special effect, it just needs to look like it’s moving fast) and at the end of the rotation period I would need it to reset to a default “starting position”.
The smaller the motor the better as I would like it to be wearable on the wrist. Could support suggest a servo motor that meets these specs?
Hello @derrick.nhan
This link is the smallest continuous rotation servo motors we carry.
Hello. According to the datasheet for ConnectorCore 6UL modules (Level 3 MSL) they have an expected shelf life of 12 months.
If we are to use them past their expiration, what should we do to the material? Would baking the pieces for 4 to 6 hours at 125 C be enough? What other recommendations should we take into consideration?
Thank you.
You would need to use the body thickness of the ConnectorCore 6UL modules, which is 3.5mm, to determine the baking temperature and times.
Here is a link to our forum page for baking times and temperatures:
Hi there, I want to ask about the MTBP of PBO-5C-5 unit produced by CUI Inc… The Datasheet lists it as 1,000,000 hr, but I want a more accurate result cause I have to test it. can you share that report with me if it exists?
Hello hrjo,
Welcome to the DigiKey TechForum.
I think you mean MTBF (Mean Time Between Failure), I’m not sure what MTBP is. And yes MTBF for PBO-5C-5 is listed as 1,000,000 hours according to the data sheet but unfortunately we don’t have a specific report on that. If there is one it is likely with the manufacturer of this device CUI Inc. However, they may not be able to share that and we would have to see if we can obtain it from them through our product management team.
There is info on MTBF in the data sheet in regards to safety and compliance table page 2:

Maybe that helps.
If you would still like us to try and obtain that report from CUI Inc. please let us know. Do give us your email to send that report to if we do obtain it.
Welcome to the Technical Forum. I can find the 275T series on this link: https://deltrol-controls.com/sites/default/files/pdf/data-sheet/270-275%20Series%20Data%20Sheet.pdf
I could not find te part number of 23246-70 on a data sheet to really tell me what the part is. We would need more information unless someone else can figure it out. There are others moitoring this forum. So maybe more help will be found. The second relay I can’t see with the glare. We need a better picture on that one.