We use cookies to provide our visitors with an optimal site experience. View our privacy notice and cookie notice to learn more about how we use cookies and how to manage your settings. By proceeding on our website you consent to the use of cookies.
We are building a custom Ubuntu 16.04 image on a BeableBone black derived project (as in our own board). We have used omap-image-builder-v2018.01 as the base for the distribution. It compiles fine and we habe been using the image since the beginning of the year for development.
Recently, we added some logging using spdlog. However, it requires an update to libstdc++6 as the version in the xenial repos is not at the same version as that required by spdlog. We can manually update the library doing the following:
###Needed for add-apt-repository
sudo apt install -y software-properties-common
Recommended by source but not something we want to do.
#sudo apt-get upgrade
Instead we do this
sudo apt install libstdc++6
The procdure above works on our target. However, we want to add this to the image. I tried modifying the chroot.sh script in the scripts folder doing this:
if [ "x${enable_ppa_launchpad}" = "xenable" ] ; then
## this one comes for the internet, not the proxy !!!
apt-get -y \${apt_options} install software-properties-common || true
echo "Log: (chroot) add-apt-repository -y ppa:ubuntu-toolchain-r/test"
add-apt-repository -y ppa:ubuntu-toolchain-r/test
#Disable by RobertCNelson
#patch_launchpad_sources_list
## Only update the PPA sources
apt-get update -o Dir::Etc::sourcelist="sources.list.d/ubuntu-toolchain-r-ubuntu-test-xenial.list" -o Dir::Etc::sourceparts="-" -o APT::Get::List-Cleanup="0"
if [ ! "x${ppa_launchpad_pkg_list}" = "x" ] ; then
echo "Log: (chroot) Installing (from ppa.launchpad.net): ${ppa_launchpad_pkg_list}"
#Missing install.... by RobertCNelson
apt-get -y install ${ppa_launchpad_pkg_list}
fi
fi
The add-apt-ropository command adds the file /etc/apt/sources.list.d/ubuntu-toolchain-r-ubuntu-test-xenial.list
Which contains:
deb Index of /ubuntu-toolchain-r/test/ubuntu xenial main
Log: (chroot) add-apt-repository -y ppa:ubuntu-toolchain-r/test
gpg: keyring `/tmp/tmpna61yach/secring.gpg' created
gpg: keyring `/tmp/tmpna61yach/pubring.gpg' created
gpg: requesting key BA9EF27F from hkp server keyserver.ubuntu.com
gpg: /tmp/tmpna61yach/trustdb.gpg: trustdb created
gpg: key BA9EF27F: public key "Launchpad Toolchain builds" imported
gpg: Total number processed: 1
gpg: imported: 1 (RSA: 1)
OK
Get:1 http://ppa.launchpad.net/ubuntu-toolchain-r/test/ubuntu xenial InRelease [17.5 kB]
Get:2 http://ppa.launchpad.net/ubuntu-toolchain-r/test/ubuntu xenial/main armhf Packages [60.8 kB]
Fetched 78.3 kB in 2s (35.3 kB/s)
Reading package lists... Done
Log: (chroot) Installing (from ppa.launchpad.net): libstdc++6
Reading package lists... Done
Building dependency tree
Reading state information... Done
The following additional packages will be installed:
gcc-8-base
The following NEW packages will be installed:
gcc-8-base
The following packages will be upgraded:
libstdc++6
1 upgraded, 1 newly installed, 0 to remove and 13 not upgraded.
Need to get 376 kB of archives.
After this operation, 155 kB of additional disk space will be used.
Get:1 http://ppa.launchpad.net/ubuntu-toolchain-r/test/ubuntu xenial/main armhf gcc-8-base armhf 8.1.0-5ubuntu1~16.04 [18.5 kB]
Get:2 http://ppa.launchpad.net/ubuntu-toolchain-r/test/ubuntu xenial/main armhf libstdc++6 armhf 8.1.0-5ubuntu1~16.04 [357 kB]
Fetched 376 kB in 1s (323 kB/s)
Selecting previously unselected package gcc-8-base:armhf.
(Reading database ... 31451 files and directories currently installed.)
Preparing to unpack .../gcc-8-base_8.1.0-5ubuntu1~16.04_armhf.deb ...
Unpacking gcc-8-base:armhf (8.1.0-5ubuntu1~16.04) ...
Setting up gcc-8-base:armhf (8.1.0-5ubuntu1~16.04) ...
(Reading database ... 31457 files and directories currently installed.)
Preparing to unpack .../libstdc++6_8.1.0-5ubuntu1~16.04_armhf.deb ...
Unpacking libstdc++6:armhf (8.1.0-5ubuntu1~16.04) over (5.4.0-6ubuntu1~16.04.10) ...
Processing triggers for libc-bin (2.23-0ubuntu10) ...
Setting up libstdc++6:armhf (8.1.0-5ubuntu1~16.04) ...
Processing triggers for libc-bin (2.23-0ubuntu10) ...
Here is the full diff, i no longer have “xenial” support in the git repo, so there was a few things to add back apt_options…
diff --git a/scripts/chroot.sh b/scripts/chroot.sh
index d1590c2f..63916e08 100755
--- a/scripts/chroot.sh
+++ b/scripts/chroot.sh
@@ -562,6 +562,12 @@ cat > "${DIR}/chroot_script.sh" <<-__EOF__
dpkg-divert --local --rename --add /sbin/initctl
ln -s /bin/true /sbin/initctl
fi
+
+ apt_options=""
+ if [ "x\${deb_codename}" = "xxenial" ] ; then
+ apt_options="--allow-downgrades --allow-remove-essential --allow-change-held-packages"
+ fi
+ echo "Log: (chroot): apt using extra: [\${apt_options}]"
}
install_pkg_updates () {
@@ -594,8 +600,8 @@ cat > "${DIR}/chroot_script.sh" <<-__EOF__
fi
apt-get update
- apt-get upgrade -y
- apt-get dist-upgrade -y
+ apt-get upgrade -y \${apt_options}
+ apt-get dist-upgrade -y \${apt_options}
if [ ! -f /etc/resolv.conf ] ; then
#'/etc/resolv.conf.bak' -> '/etc/resolv.conf'
@@ -647,7 +653,7 @@ cat > "${DIR}/chroot_script.sh" <<-__EOF__
#Install the user choosen list.
echo "Log: (chroot) Installing: ${deb_additional_pkgs}"
apt-get update
- apt-get -y install ${deb_additional_pkgs}
+ apt-get -y \${apt_options} install ${deb_additional_pkgs}
fi
if [ "x${chroot_enable_debian_backports}" = "xenable" ] ; then
@@ -659,7 +665,7 @@ cat > "${DIR}/chroot_script.sh" <<-__EOF__
if [ ! "x${repo_external_pkg_list}" = "x" ] ; then
echo "Log: (chroot) Installing (from external repo): ${repo_external_pkg_list}"
- apt-get -y install ${repo_external_pkg_list}
+ apt-get -y \${apt_options} install ${repo_external_pkg_list}
fi
if [ ! "x${repo_ros_pkg_list}" = "x" ] ; then
@@ -674,12 +680,28 @@ cat > "${DIR}/chroot_script.sh" <<-__EOF__
apt-mark hold chromium || true
fi
+ if [ "x${enable_ppa_launchpad}" = "xenable" ] ; then
+ ## this one comes for the internet, not the proxy !!!
+ apt-get -y \${apt_options} install software-properties-common || true
+
+ echo "Log: (chroot) add-apt-repository -y ppa:ubuntu-toolchain-r/test"
+ add-apt-repository -y ppa:ubuntu-toolchain-r/test
+
+ ## Only update the PPA sources
+ apt-get update -o Dir::Etc::sourcelist="sources.list.d/ubuntu-toolchain-r-ubuntu-test-xenial.list" -o Dir::Etc::sourceparts="-" -o APT::Get::List-Cleanup="0"
+
+ if [ ! "x${ppa_launchpad_pkg_list}" = "x" ] ; then
+ echo "Log: (chroot) Installing (from ppa.launchpad.net): ${ppa_launchpad_pkg_list}"
+ apt-get -y \${apt_options} install ${ppa_launchpad_pkg_list} || true
+ fi
+ fi
+
##Install last...
if [ ! "x${repo_rcnee_pkg_version}" = "x" ] ; then
echo "Log: (chroot) Installing modules for: ${repo_rcnee_pkg_version}"
- apt-get -y install libpruio-modules-${repo_rcnee_pkg_version} || true
- apt-get -y install rtl8723bu-modules-${repo_rcnee_pkg_version} || true
- apt-get -y install ti-cmem-modules-${repo_rcnee_pkg_version} || true
+ apt-get -y \${apt_options} install libpruio-modules-${repo_rcnee_pkg_version} || true
+ apt-get -y \${apt_options} install rtl8723bu-modules-${repo_rcnee_pkg_version} || true
+ apt-get -y \${apt_options} install ti-cmem-modules-${repo_rcnee_pkg_version} || true
depmod -a ${repo_rcnee_pkg_version}
update-initramfs -u -k ${repo_rcnee_pkg_version}
fi
So to resume, missing install and repo_rcnee_pkg_version must be last.
Your base seems different from mine.
Did you add the changes to install_pkgs_update () ?
But mine was in install_pkgs ()
I will grab the latest version of chroot in https://rcn-ee.com/rootfs/eewiki/minfs/ubuntu-18.04.1-minimal-armhf-2018-07-30.tar.xz and apply the patch to it. So that I cab make the correct comparison and backport the changes to my version !
But since yours work, I will stick as closely as possible to yours. I will give you my results as soon as I have done it !
Correct, that was from git master https://github.com/RobertCNelson/omap-image-builder. I added the call into install_pkgs_updates, vs install_pkgs, as to minimize any issues with a newer libc when installing packages built against the old library.
The repo at ppa.launchpad is not providing the file Packages for armhf. Which then makes it impossible to get the libstdc++6 package. Since the same commands work on the target and libstdc++6 is pulled it then it’s not a case of ppa.launchpad not having the file. It must be something with my build setup. Also since your version works it points to other differences in my build process. Here is the error log:
[Note I had to break the links below to publish this. Not allowed to put more than 2 links, all the htp were actually http]
gpg: keyring `/tmp/tmpu4lgddej/pubring.gpg’ created
gpg: requesting key BA9EF27F from hkp server keyserver.ubuntu.com
gpg: /tmp/tmpu4lgddej/trustdb.gpg: trustdb created
gpg: key BA9EF27F: public key “Launchpad Toolchain builds” imported
gpg: Total number processed: 1
gpg: imported: 1 (RSA: 1)
OK
Ign:1 htp://ppa.launchpad.net/ubuntu-toolchain-r/test/ubuntu xenial InRelease
Ign:2 htp://ppa.launchpad.net/ubuntu-toolchain-r/test/ubuntu xenial Release
Ign:3 htp://ppa.launchpad.net/ubuntu-toolchain-r/test/ubuntu xenial/main armhf Packages
Ign:4 htp://ppa.launchpad.net/ubuntu-toolchain-r/test/ubuntu xenial/main all Packages
Ign:5 htp://ppa.launchpad.net/ubuntu-toolchain-r/test/ubuntu xenial/main Translation-en
Ign:3 htp://ppa.launchpad.net/ubuntu-toolchain-r/test/ubuntu xenial/main armhf Packages
Ign:4 htp://ppa.launchpad.net/ubuntu-toolchain-r/test/ubuntu xenial/main all Packages
Ign:5 htp://ppa.launchpad.net/ubuntu-toolchain-r/test/ubuntu xenial/main Translation-en
Ign:3 htp://ppa.launchpad.net/ubuntu-toolchain-r/test/ubuntu xenial/main armhf Packages
Ign:4 htp://ppa.launchpad.net/ubuntu-toolchain-r/test/ubuntu xenial/main all Packages
Ign:5 htp://ppa.launchpad.net/ubuntu-toolchain-r/test/ubuntu xenial/main Translation-en
Ign:3 htp://ppa.launchpad.net/ubuntu-toolchain-r/test/ubuntu xenial/main armhf Packages
Ign:4 htp://ppa.launchpad.net/ubuntu-toolchain-r/test/ubuntu xenial/main all Packages
Ign:5 htp://ppa.launchpad.net/ubuntu-toolchain-r/test/ubuntu xenial/main Translation-en
Ign:3 htp://ppa.launchpad.net/ubuntu-toolchain-r/test/ubuntu xenial/main armhf Packages
Ign:4 htp://ppa.launchpad.net/ubuntu-toolchain-r/test/ubuntu xenial/main all Packages
Ign:5 htp://ppa.launchpad.net/ubuntu-toolchain-r/test/ubuntu xenial/main Translation-en
Err:3 htp://ppa.launchpad.net/ubuntu-toolchain-r/test/ubuntu xenial/main armhf Packages
404 Not Found
Ign:4 htp://ppa.launchpad.net/ubuntu-toolchain-r/test/ubuntu xenial/main all Packages
Ign:5 htp://ppa.launchpad.net/ubuntu-toolchain-r/test/ubuntu xenial/main Translation-en
Reading package lists… Done
W: Can’t drop privileges for downloading as file ‘/var/lib/apt/lists/partial/ppa.launchpad.net_ubuntu-toolchain-r_test_ubuntu_dists_xenial_InRelease’ couldn’t be accessed by user ‘_apt’. - pkgAcquire::Run (13: Permission denied)
W: The repository ‘htp://ppa.launchpad.net/ubuntu-toolchain-r/test/ubuntu xenial Release’ does not have a Release file.
N: Data from such a repository can’t be authenticated and is therefore potentially dangerous to use.
N: See apt-secure(8) manpage for repository creation and user configuration details.
E: Failed to fetch htp://ppa.launchpad.net/ubuntu-toolchain-r/test/ubuntu/dists/xenial/main/binary-armhf/Packages 404 Not Found
E: Some index files failed to download. They have been ignored, or old ones used instead.
Log: umount: [/home/wdurocher/ArmLinux/LF102/Distro/Ubuntu/omap-image-builder-v2018.01/ignore/tmp.psg89YB6Mm/dev/pts]
Log: umount: [/home/wdurocher/ArmLinux/LF102/Distro/Ubuntu/omap-image-builder-v2018.01/ignore/tmp.psg89YB6Mm/proc]
Log: umount: [/home/wdurocher/ArmLinux/LF102/Distro/Ubuntu/omap-image-builder-v2018.01/ignore/tmp.psg89YB6Mm/sys]
Log: umount: [/home/wdurocher/ArmLinux/LF102/Distro/Ubuntu/omap-image-builder-v2018.01/ignore/tmp.psg89YB6Mm/run]
Here is what I think may be an issue:
I am using a proxy (mirror of sources) for the regular build (we want to freeze the packages we use to build to a specific version). It is still possible to build from the internet though.
Indeed, the use of the proxy is preventing ppa.launchpad from being reached. When I build from the internet sources the build proceeds to the endI will have to fix that issue.
But in the mean time the problem I initially opened has been fixed
I am using apt-mirror and created a mirror of:
ports. ubuntu. com xenial and xenial-updates in main, universe and multiverse
As well as repos. rcn-ee. com/ubuntu xenial main
I did have to do some dancing to get the script to access the repos as http://192.168.1.228/[Actual repo URL]
The apt_proxy was not working otherwise.